2021-08-26 11:13 AM
Can i replace the stm32f427vit6 with the f429vit6, f437vit6 or 439vit6 without changing code, and are they completely pin compatible?
Solved! Go to Solution.
2021-08-26 11:24 AM
Yes. The F429 and F439 have LCD. The F437 and F439 have crypto. The F427 has neither of these but is otherwise identical.
The "List Pinout Compatible MCUs" feature in CubeMX can be used to answer questions like these.
2021-08-26 11:24 AM
Yes. The F429 and F439 have LCD. The F437 and F439 have crypto. The F427 has neither of these but is otherwise identical.
The "List Pinout Compatible MCUs" feature in CubeMX can be used to answer questions like these.
2021-08-26 11:26 AM
Thanks you 👍🏻
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.