STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Octo-SPI memory-mapped mode speed for H735

Hi,We are using the OCTOSPI2 on a H735 in memory map mode.We are copying 32 bits values one by one, from the internal RAM to the Octo memory.We transfer around 5000 x 32 bits in 2ms which is around 10MB/s.I think, it is a bit slow. What is the maximu...

Resolved! Using OCTOSPI in Memory Mapped mode with an QuadSPI SRAM

Hi guys,I am using an STM32L552ZET6 and I would like to extend the RAM using an external SRAM chip (23A1024-E/TS), that has an QuadSPI interface. I would like to know if I can use STM32L5 OCTOSPI interface in memory mapped mode with the above mention...

CDan.1 by Associate II
  • 2020 Views
  • 3 replies
  • 0 kudos

STM32F103 upper flash pages corrupted/erased.

Dear ST community,I was wondering if you could help me with a problem I'm having with an STM32. I have a system containing an STM32F103VET6. The last flash pages are used to store settings/parameters. 2 redundant flash pages are used. This system...

Switching Port Pins between Alt Function and Normal mode

Hi All,In a situation where someone might be flashing an LED using a Timer Output (eg Alternate Function Mode connected to a Timer channel output), what if you want to then turn the LED on solid or totally off and then maybe back to the Timer flashin...

RMyer.1 by Associate III
  • 2761 Views
  • 6 replies
  • 0 kudos

STM32H747 HSEM issue

Hello,I am trying to manage data transfer between the 2 core of the STM32H747.My problem is all hardware semaphore are locked just at the initialisation phase ( MASTERID 0X03 , Core M7) After Hal_Init(); & SystemClock_Config(); all is free.after __HA...

Configuring OCTOSPI on a STM32H723/STM32H730

I'm having an issue configuring the OCTOSPI for accessing an external HyperRAM (Cypress S27KL0643) connected to OCTOSPI1.My basic issue is that the STM32 doesn't provide a chip select or clock when I attempt to access the chip.I'm suspect I'm misconf...

0693W00000DqN0KQAV.png
JCoop.2 by Associate
  • 3565 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32f427vit6 replacement

Can i replace the stm32f427vit6 with the f429vit6, f437vit6 or 439vit6 without changing code, and are they completely pin compatible?​​​

DSmit.111 by Associate II
  • 1730 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.