2025-12-26 7:12 AM
Hello everyone,
This is my first post on the ST Community forum.
I recently moved from a custom 6-layer board using STM32H725IGKB to a simpler 4-layer board using STM32H723ZGT6. Both designs use an external OCTOSPI memory, with 50 ohm controlled-impedance routing and 33 ohm series resistors on the signals.
On the new 4-layer board, I am seeing read/write errors on the OCTOSPI interface, while the original 6-layer board works reliably with similar routing and firmware.
I would like to ask whether the OCTOSPI output driver characteristics or output impedance differ between STM32H725 and STM32H723, or if these issues are more likely related to signal integrity, stack-up, or return-path differences on a 4-layer PCB.
Any guidance or experience would be appreciated.
Thank you in advance.
Solved! Go to Solution.
2025-12-26 7:19 AM - edited 2025-12-26 7:20 AM
Hello @Jonshill and welcome to the ST community,
I think better to start to read this application note: AN4803 "High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs" and use IBIS information with HyperLynx tool and run simulations.
2025-12-26 7:19 AM - edited 2025-12-26 7:20 AM
Hello @Jonshill and welcome to the ST community,
I think better to start to read this application note: AN4803 "High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs" and use IBIS information with HyperLynx tool and run simulations.
2025-12-27 1:29 AM
Thanks for the suggestion. I’ll go through AN4803 and look into running IBIS-based simulations with the HyperLynx SI tool to better understand the signal integrity aspects on this new board.
Quick question: when using the HyperLynx tool with the STM32 IBIS models, are there any common pitfalls or specific settings you recommend for STM32H7 devices that I should pay attention to?
2025-12-27 5:36 AM
Nothing special to STM32H7. That application note provides STM32F7 and STM32MP15 but as examples. STM32F7 as a microcontroller and STM32MP15 as a microprocessor. The same process should applies to STM32H7.
If I answerd your original question please accept my previous post as solution.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.