2018-04-11 5:23 PM
I am using an STM32F446ZE Nucleo Board which does NOT have an external HSE clock. From CubeMX I set the clock input from the HSE and after in the clock configuration I set the system clock to 180MHz.
https://i.stack.imgur.com/JyaEk.png
and in the clock configuration I set the PLL like this
https://i.stack.imgur.com/bxOm4.png
The code generated by CubeMX seems to be correct also.
My point is that even if I don't have an HSE in the board the uController works in 180MHz. How is this possible? What is the clock input after all?2019-03-27 9:07 AM
Make sure you are using the HSE in BYPASS mode in the clock settings.
You have to start the HSE, it will not start oscillating automatically. ie HSE_ON
If it doesn't oscillate most likely that your circuit characteristics are wrong.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.