STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

arbitrary waveform using DMA and timer

Hello,i am trying to generate arbitrary waveform. But it still dose not work. I think it's up to the configuration. I have created a array of 6 words for two waveform patterns to be send to TIM1 channel 1 (TIM1_ARR, TIM1_RCR, TIM1_CCR1) This is how t...

Samuel1 by Associate III
  • 7978 Views
  • 7 replies
  • 0 kudos

Resolved! LPUART RX DMA Configured But Does Not Start!

Hello:I seemingly have the LPUART now configured correctly. For sure the transmit (without DMA) functions OK. I only have receive DMA configured. As usual, it was done in Cube.uint8_t rxBuff[40];#define RX_DMA_SZ 10The start is the same as I am using...

STM32L452 + SD + DMA + FATFS + STM32CubeMX v5.0.0: DMA and SD interrupts can signal end of transfer before it's complete

We are using an STM32L452, running directly from an HSE crystal at 8 MHz (i.e. no PLL), using the SDMMC peripheral with an SD clock of 8 MHz, and DMA for transferring data to and from SDMMC.When the DMA part of an SD read is complete, HAL_DMA_IRQHand...

STM32F4 HSE clock frequency without HSE

Posted on April 12, 2018 at 02:23I am using an STM32F446ZE Nucleo Board which does NOT have an external HSE clock. From CubeMX I set the clock input from the HSE and after in the clock configuration I set the system clock to 180MHz.https://i.stack.i...

Error compiling for board Nucleo-64 with Arduino IDE

Hello,I tried to compile the simple "Blink" sample with the Arduino IDE, but I get always an error:Board Nucleo_64 (platform stm32, package STM32) is unknown Error compiling for board Nucleo-64.I installed the latest Stm32 Cores (1.3.0) via the Boa...

EKars by Associate
  • 2614 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.