2017-06-29 5:30 AM
I try to make some noise using a small 8 OHm @ 1 kHz Buzzer connected to the STM32F446 DAC_OUT1. Seams the PA4 pin got damaged due to high or reverse voltage induced by the buzzer. I used th push/pull GPIO config. Is it possible to directly drive this buzzer without an external PA IC maybe by enabling the internal DAC-Buffer? Or is it required to drive the buzzer via an PA? Or would the IO cell get damaged due to high or reverse voltage induced by the speakers large inductance?
2017-06-29 5:52 AM
The buffer won't give enough energy to directly drive a speaker, you'll need an external audio booster.
A digital GPIO with square waves might be able to drive some piezo with low volume. At 3V x 5mA = 15mW DC
2017-06-29 6:12 AM
Is it possible to directly drive this buzzer without an external PA IC maybe by enabling the internal DAC-Buffer?
Only if you find a buzzer with 15k Ohm impedance...
2017-06-29 9:52 AM
But isn't it dangerous to connect such a large coil directly to the processors pin? I suspect the pin could be damaged through induced high or reverse voltage. Am I wrong?
2017-06-29 10:43 AM
Piezo buzzer usually have no coils, AFAIK.
But first find one with 15k impedance ...
What I meant to say - in practical terms, you cannot connect a speaker/buzzer to ST's DAC (and get useful output).
The power output would be less than 1 milliWatt ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.