cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer CLI v2.19.0 — Cannot program second double-word of an OTP row (STM32U385)

murali.karicheri
Associate III

Product/Tool: STM32CubeProgrammer CLI v2.19.0
Target MCU: STM32U385RG-Q (Nucleo-U385RG-Q board)
Connection: SWD, mode=UR (Under Reset)
TZEN: 0 (non-secure)

================================================================================
SUMMARY
================================================================================

We are unable to program a full 16-byte OTP row using STM32_Programmer_CLI.
Only the first double-word (8 bytes) of a row can be written. Any attempt to
program the second double-word of the same row fails silently (word remains
0xFFFFFFFF) or is rejected by the flash controller, even though the row should
not be locked until both double-words are programmed.

Per the reference manual, the OTP lock granularity is one 16-byte row
(2 double-words). We expect to be able to program both double-words within a
row independently (each in a single operation), provided neither has been
written previously. However in practice, programming the first double-word
appears to immediately lock the entire row, preventing the second double-word
from being written.

================================================================================
OTP ADDRESS LAYOUT
================================================================================

- OTP base: 0x0BFA0000
- Each row: 16 bytes = 2 double-words (DW0 at offset+0, DW1 at offset+8)
- Example: Row at offset 160 -> DW0 = 0x0BFA00A0, DW1 = 0x0BFA00A8

================================================================================
WHAT WE TRIED
================================================================================

All commands below use:

STM32_Programmer_CLI -c port=SWD mode=UR

--------------------------------------------------------------------------------
Attempt 1: Two separate -w32 commands (2 words each)
--------------------------------------------------------------------------------

# Program first double-word (offset 160) — SUCCEEDS
STM32_Programmer_CLI -c port=SWD mode=UR -w32 0x0BFA00A0 0x33323130 0x00003534

# Program second double-word (offset 168) — FAILS (stays 0xFFFFFFFF)
STM32_Programmer_CLI -c port=SWD mode=UR -w32 0x0BFA00A8 0xDEADBEEF 0xCAFEBABE

Readback after both commands shows DW0 programmed correctly, DW1 remains
0xFFFFFFFF FFFFFFFF.

--------------------------------------------------------------------------------
Attempt 2: Single -w32 command with 4 words (16 bytes)
--------------------------------------------------------------------------------

# Write all 4 words in one command
STM32_Programmer_CLI -c port=SWD mode=UR \
-w32 0x0BFA00A0 0x33323130 0x00003534 0xDEADBEEF 0xCAFEBABE

Result: Only the first 2 words (DW0) are programmed. The second 2 words (DW1)
remain 0xFFFFFFFF.

--------------------------------------------------------------------------------
Attempt 3: Binary file write (-w with .bin file)
--------------------------------------------------------------------------------

Created a 16-byte binary file containing the desired data and wrote it:

STM32_Programmer_CLI -c port=SWD mode=UR -w 0x0BFA00A0 otp_data.bin

Result: Same — only the first 8 bytes are written.

--------------------------------------------------------------------------------
Attempt 4: Chained commands in one invocation
--------------------------------------------------------------------------------

STM32_Programmer_CLI -c port=SWD mode=UR \
-w32 0x0BFA00A0 0x33323130 0x00003534 \
-w32 0x0BFA00A8 0xDEADBEEF 0xCAFEBABE

Result: First double-word succeeds, second double-word fails.

--------------------------------------------------------------------------------
Attempt 5: Different row to rule out damaged OTP
--------------------------------------------------------------------------------

Moved to offset 176 (a fresh row) and successfully programmed DW0. Confirmed
the previous row (160) failure is repeatable on multiple fresh rows — only DW0
can be written.

================================================================================
VERIFICATION
================================================================================

Reading via:

STM32_Programmer_CLI -c port=SWD mode=UR -r32 0x0BFA00A0 4

Consistently shows the first 2 words written correctly and the last 2 words
as 0xFFFFFFFF.

================================================================================
QUESTIONS
================================================================================

1. Is this a known limitation of the STM32U3 OTP or the flash controller
when TZEN=0?

2. Is there a required sequence (e.g., specific register unlocking, delay
between double-words, or a different programming mode) to write the second
double-word of an OTP row?

3. Does STM32CubeProgrammer internally lock the row after programming the
first double-word? If so, is there a CLI flag or workaround to defer row
locking?

4. Is this addressed in a newer version of STM32CubeProgrammer?

================================================================================
ENVIRONMENT
================================================================================

- STM32CubeProgrammer: v2.19.0 (Linux x86_64)
- Board: NUCLEO-U385RG-Q
- MCU: STM32U385RGT6
- TZEN: 0
- Connection: SWD via ST-LINK, mode=UR

1 ACCEPTED SOLUTION

Accepted Solutions
Aziz BRIGUI
ST Employee

Hi @murali.karicheri

This issue was detected internally and was fixed in STM32CubeProgrammer v2.22.0. Could you try and confirm on your side?

Aziz

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Aziz BRIGUI
ST Employee

Hi @murali.karicheri

This issue was detected internally and was fixed in STM32CubeProgrammer v2.22.0. Could you try and confirm on your side?

Aziz

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Aziz,

Thanks for your quick response and support. Confirm that v2.22.0 has fixed the bug. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.