STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 f4xxx: how did I end up in reset_handler?

Posted on June 29, 2017 at 17:56HiIn which cortex registers would I see where this reset originated from?I have a breakpoint in the CUBEMX resethandler.Which gets trigerred after some seconds. My Project: UDP loopback LWIP + freertos. The reset happ...

IAR 7.80.2 can't download to STM32F427

Posted on June 22, 2017 at 22:25I have a customer made board with cpu STM32F427VG and ST-LINK V2 debugger, , IAR 7.80.2 can't download , but ST-LINK utility sometimes can and sometimes fail, please see the following. thanks very much for your help1....

0690X00000607TEQAY.png 0690X00000607TdQAI.png 0690X00000607T4QAI.png

DMA transfers 25% of buffer in memory to memory mode

Posted on June 29, 2017 at 23:46Using STM32F417 DMA and got it to work but it only transfers 25% of the buffer size indicated. So far, I have tested the following buffer sizes:Buffer size (bytes)            Bytes transferred10                       ...

Encoder mode with LOW POWER TIMER 1

Posted on June 16, 2017 at 00:32STM32L476I can't seem to glean the needed settings from the RM0351 rev 5 to get this to work like I thought it would.It seems to somewhat work but I can't get any counting to happen with transitions on input 1 (PC0). ...

Auto Wake-up for STM32F042

Posted on June 28, 2017 at 18:41Hi everybody,I'm wondering why the HAL library does not allow to program an auto wakeup for a STM32F042.It is not allowed via CubeMX GUI neither.I've looked into hal files :every function used to init/use the auto wak...

Resolved! HAL geniuses, how does this work?

Posted on June 16, 2017 at 23:56From the STM32F412G-DISCO demouint32_t HAL_GetTick(void){ return (DWT->CYCCNT / (HAL_RCC_GetHCLKFreq() / 1000)) ;}How exactly does this wrap properly within the 32-bit number space? Answer: IT DOESN'T

STM32CubeMX HCLK clock configuration 30MHz limit

Posted on May 23, 2017 at 10:55Hello,I am trying to reduce the HCLK frequency down to 8MHz or less on an STM32F405 MCU.Using STM32CubeMX, when I configure an HCLK clock lower than 30MHz with the clock configuration tool, the box with the HCLK freque...

Dulan D by Associate II
  • 3218 Views
  • 7 replies
  • 0 kudos

STM32L476 on NUCLEO-L476RG Baudrate with CubeMX

Posted on June 29, 2017 at 16:01Configured USART1 of mcu to 500 kbit/sec using STM32CubeMX Version 4.21.0.Code created by Cube seems to be correct.Measurement shows that bitrate is 250 kbit ( a 10 bit character needs 40 µsec).See Attachements.USART...

JuM by Senior
  • 1212 Views
  • 1 replies
  • 0 kudos

STM32F469I-DISCO - CubeMX project file for LCD

Posted on June 29, 2017 at 08:03Hi,I prepared several project files for a few DISCOVERY boards (I shared examples for STMF429, STM32F746, STM32F412, etc), but this time it seems to take more time than I expected. Maybe someone from you guys already ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.