2017-01-23 5:57 AM
Hello,
i want a baud rate of 5 mbps on UART1/UART6 on STM32F207 Nucleo Board (As per reference Manual UART1 & UART6 can have baud rate up to 7.5 Mbps). However when i am configuring in STM Cube MX i am getting baud rate of 3.7 mbps max for both UART1 & UART6. I have checked clock configuration many times.
HCLK= 120 MHz, APB1= 30MHz, APB2=60 MHz exactly. In Addition to this i also tried to give Input frequency of 25MHz (26 MHz max).
Still i am unable to cross 3.7 Mbps (max possible value as per Cube Mx)
So can anybody suggest me possible solution??.
#stm32f207-uart2017-01-23 8:15 AM
Thank you..Got it..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.