STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in STM32L4xx_HAL_Driver (SPI Transmit)

Posted on March 21, 2016 at 13:30 Component: STM32L4xx_HAL_Driver File: stm32l4xx_hal_spi.c Function: HAL_SPI_Transmit Line number: 519 Description: SPI RX FIFO not empty after transmit. Solution: Remove { __HAL_SPI_CLEAR_O...

STM32F207 Nucleo 144 UART1 Baud Rate

Posted on January 23, 2017 at 14:57Hello,i want a baud rate of 5 mbps on UART1/UART6 on STM32F207 Nucleo Board (As per reference Manual UART1 & UART6 can have baud rate up to 7.5 Mbps). However when i am configuring in STM Cube MX i am getting baud ...

USB problems

Posted on January 05, 2017 at 13:59Hello,I use a TUSB2046BVF to connect a host (tablet) to 2 USB connectors and 2 micros, one is STM32F103 and the otherSTM32F107, and I can only operate the 103 when I remove the pull-up resistor at 107.The other por...

STM32CubeF1 startup file

Posted on January 21, 2017 at 18:40Hi,I downloaded stm32cubef1 firmware package.  I am using examples on STM3210E_EVAL projects.  With the EWARM(IAR embedded workbend for ARM), I see all examples use startup_stm32f103xg.s as start up file.I am using...

Jian Chen by Associate II
  • 1173 Views
  • 1 replies
  • 0 kudos

Preferred method for determing hardware at runtime?

Posted on January 21, 2017 at 04:50You want us to use the HAL, ok fine.  We use the HAL. But we still often times need to know what hardware we are running on. What is the factory approved method for determining which board/chip is running?Where is ...

stm32 can1 cannot receive 22 frame messages totally

Posted on January 23, 2017 at 09:29Hi guys:There are 1 master and 22 slaves,both cpu are stm32,The 22 salves address are 1.2……22,The address number are included in the can Extend ID.The master has 2 cans, can1 and can2.When the master sent the query...

BeMercy by Associate II
  • 748 Views
  • 0 replies
  • 0 kudos

ADC I2C Problem

Posted on January 18, 2017 at 03:16HelloI have project MP3 using STM32F030C8.MP3 decoder using I2C interface and user key using ADC. So, beginning of my prototype use STM32L0 series, it already done and no problem at all. After that I change to STM3...

0690X00000605vDQAQ.png 0690X00000603YtQAI.jpg 0690X00000603YyQAI.jpg
dree86 by Associate II
  • 3106 Views
  • 5 replies
  • 0 kudos

How to Reset the DMA receiving buffer

Posted on January 23, 2017 at 00:31 I am not dealing with continuous streaming of data, I just send a command to the connected device and wait a reply on the UART using DMA. Now using DMA I can only start seeing data after a while, say 1sec!!. I ...

Raider E by Associate III
  • 1106 Views
  • 0 replies
  • 0 kudos

ADC cannot read multiple channels ..

Posted on December 16, 2016 at 00:08The original post was too long to process during our migration. Please click on the attachment to read the original post.

Raider E by Associate III
  • 3293 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.