cancel
Showing results for 
Search instead for 
Did you mean: 

failed to start GDB server

Charan_sahoo
Associate

Hello everyone,

I am facing a flashing/debugging issue with the STEVAL-SPIN3202 Rev 3.1 board.

Board:
STEVAL-SPIN3202 Rev 3.1

Software Used:

  • STM32CubeIDE

  • STM32CubeProgrammer

Problem:
While trying to flash or debug the board from STM32CubeIDE, I get the following error:

"Failed to start GDB server"
"Error in initializing ST-LINK device"
"Failed to connect to device"

Also, in STM32CubeProgrammer:

  • Read data operation fails

  • Target connection sometimes not detected

Additional Observations:

  • ST-LINK USB is detected intermittently

  • Board LED becomes dim/slow ON sometimes

  • Reinstalled STM32CubeIDE and drivers

  • Installed ST-LINK drivers

  • Tried different USB cables and USB ports

  • Tried lower SWD frequency

  • Tried Hot Plug mode

  • Tried BOOT0 method

  • Still unable to flash or read target

I would appreciate guidance on:

  1. Correct jumper settings for STEVAL-SPIN3202 Rev 3.1

  2. Whether onboard ST-LINK firmware may be corrupted

  3. Possible hardware protection/reset issue

  4. Correct power supply requirements during flashing

Thank you.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Charan_sahoo, to the community!

Which connector on the STEVAL-SPIN3202 did you connect it to your computer?

Your third screenshot shows a Device ID of 0x410 as the target, i.e. STM32F101/F102/F103. However, the STSPIN32F0A contains an STM32F031.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.