cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with STM32H5 debug authentication

hijax_pl
Associate III

Test bed:
- Nucleo-H503 & Nucleo-H533
- Few WeAct H523 connected via Waveshare STLink v2 mini (4 wires only)
- my own H503 based controller connected via cheap STLink v2 clones (4 wires only)
- I am using STM32_Programmer_CLI v2.21.0 / Ubuntu 24.04 LTS

Idea - close MCU with password DA and regression only.

1) I have developed Python script to create password.bin and DA.obk files
2) with Nucleo-H533 everything works fine, I can place MCU in PROVISIONING state, program OBK, and do the regression immediately or after switching to CLOSED state.
3) H523 I can switch to PROVISIONING, program OBK, switch to CLOSED, but can not do any regression from any state - DISCOVER fails. Now I have 2 boards "bricked"
4) H503 similarly. I can write OTP, verify that, but after switching to PROVISION discovery fails.Here I have 3 boards "bricked"

But as I am using the same password all the time I still hope I will be able to regress every MCUs I played with.

Here is example using H523 in 0x17 state

$ STM32_Programmer_CLI -c port=swd sn=50FF6D065052784825260567 mode=hotplug -ob displ
      -------------------------------------------------------------------
                        STM32CubeProgrammer v2.21.0
      -------------------------------------------------------------------

ST-LINK SN  : 50FF6D065052784825260567
ST-LINK FW  : V2J47S7
Board       : --
Voltage     : 3.26V
SWD freq    : 4000 KHz
Connect mode: Hot Plug
Reset mode  : Software reset
Device ID   : 0x478
Revision ID : --
Device name : STM32H533/523
Flash size  : 256 KBytes
Device type : MCU
Device CPU  : Cortex-M33
BL Version  : 0xE2
SFSP Version: v1.2.0
Debug in Low Power mode enabled


UPLOADING OPTION BYTES DATA ...

  Bank          : 0x00
  Address       : 0x40022050
  Size          : 8 Bytes


And failed discovery but also regression (the same way)

~$ STM32_Programmer_CLI -c port=swd sn=50FF6D065052784825260567 mode=hotplug debugauth=2
      -------------------------------------------------------------------
                        STM32CubeProgrammer v2.21.0
      -------------------------------------------------------------------


Start Debug Authentication Sequence

Open SDM Lib
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   573 : open       : No response from the target

open_comms                    :   574 : open       : The target is unable to boot on RSS_DA or is in OPEN mode

open_comms                    :   575 : open       : Failed to open communication with the target

Error:
Debug Authentication: Discovery Failed

 What is happening? How can i overcome the problems? 
Are there any hardware related prerequisites? I.e. STLink v3 works but STLink v2, sometimes?

1 REPLY 1
Peter BENSCH
ST Employee

It is due to the clones of the ST-LINK/V2, which are not supported, as they contain at least illegal firmware and probably also a fake STM32F103. With a genuine ST-LINK, you avoid exactly these problems.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.