2016-01-05 1:36 AM
Hi ,
I have the STM3240G-Eval board and currently I'm working on a project which in it I'll need to display text in the LCD. I searched the internet for some informations to configure STM3240G-EVAL LCD (MB785 drived ILI 9325) with STM32CubeMxI know:
The MB785 can hook into by the FSMC_NORSRAM_BANK3 (PG10 : FSMC_NE3). MB785 use a 16 bits data BUS,
What interface must be choose betwenn STM32F407 and ILI9325?
--SRAM
-- LCD interface.
In BSP example we see below, but that not enough to use STM32CubeMx
Need your help please.Best Regards
Yves
2016-01-05 7:21 AM
Hi mevel.yves,
In the STM32F40G-EVAL, The 3.2� TFT color LCD connected to FSMC bus which ensure the connection to the SRAM.
LCD-TFT Controller (LTDC) can be used only with STM32F429xx/439xx devices. (mentioned in RM0090)
Ps: The JP3 and JP10 jumper that must not be fitted for SRAM and LCD application.
Using CubeMX, if you select the board STM32F40G-EVAL and you check the option ''Initialize all IP with their default Mode'', you will have the FSMC configured.
For further details refer to the following document:
http://www.st.com/st-web-ui/static/active/cn/resource/technical/document/user_manual/DM00036746.pdf
:
STM3240G-EVAL evaluation board
http://www.st.com/web/en/resource/technical/document/reference_manual/DM00031020.pdf
: Reference manual
:
TFT LCD interfacing with the high-density STM32F10xxx FSMC (applicable with STM32F40x)
- Hannibal -
2016-01-06 2:36 AM
Hi Hannibal
Thank you
. I think that theTFT LCD interfacing with the high-density STM32F103_Eval
is the same stm32F40G_eval but I have not idea to look for an application note.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.