2018-02-20 11:11 AM
Hello there.
What's the best way to burn a new firmware image (.hex file) on a STM32 target in the field? We don't need to debug. I need to be able update the device by sending a .hex file to the tech and he needs to burn it.
Thanks,
2018-02-20 11:27 AM
Depends on mode of connectivity. For USB you can use a .DFU file and DFU tools. For Serial the Flash Loader Demonstrator. For SWD/JTAG there is ST-LINK Utilities.
More ideally for field updates you own your update process, where you have a boot loader using the standard interfaces you provide the customer, and up load via you own application or X/Y-Modem in via a terminal. See IAP examples.
There is also this new tool
https://community.st.com/0D50X00009XkVu4SAF
2018-02-20 11:54 AM
Debuggers like stlink or jlink can do what you want.
Or Google production programmer.
2018-02-20 11:55 AM
the tech... needs to burn it
Be more specific about 'the tech'
Could she be equipped with an ST-Link and laptop, and just use that?
Agenuine ST-Link is only twenty quid or so; cheap (but perfectly usable) knock-offs are available on ebay and the like for under a fiver:
https://i.ebayimg.com/images/g/MvoAAOSwWWxY-UQm/s-ljpg
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.