STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MDK & HAL & __attribute

Posted on February 20, 2018 at 19:36I'm using the STM32CUBEMX which generates HAL code and keeps my code within defined comments. BUT, I need to define an __attribute statement BEFORE a HAL generated function header, but there is no /* USER CODE .. ...

Vector table relocation works only in debug mode

Posted on February 18, 2018 at 19:23Hi,I'm facing a problem with relocation of the vector table to the internal SRAM. I work with the STM32F030CCT6 (using the Ac6 System Workbench and CubeMX, with the HAL libraries 1.9.0) and I want to design a simp...

Resolved! Need help using USUART2 on STM32F303

Posted on February 16, 2018 at 22:30I'm trying to find instruction to code the usuart2 on this STM part. I using cmsis and the StdPeripheral lib. My end goal is to connect this to a virtual com port for debug. I'm using the Keil development environm...

STM32 Stane alone programmer

Posted on February 20, 2018 at 20:11Hello there.What's the best way to burn a new firmware image (.hex file) on a STM32 target in the field?   We don't need to debug.  I need to be able update the device by sending a .hex file to the tech and he nee...

STM32 while loop problem (using ADC DMA)

Posted on February 20, 2018 at 16:22Hi everyone,I'm trying to get working a very simple program on my Nucleo STM32L452RE-P but I have some unexpected problems...I'm using CubeMX with Atollic TrueStudio V9.0. I configured the ADC in DMA mode and also...

STM32H743ZI-NUCLEO UART DMA experiment for help

Posted on November 16, 2017 at 04:48The UART DMA communication experiment using STM32H743ZI-NUCLEO development board, the routine can work, but the project generated using CUBEMX (V4.23) and STM32CubeH7 Firmware Package V1.1.0 can not work, the perf...

one V by Associate III
  • 2772 Views
  • 6 replies
  • 0 kudos

Mapping SPI SDRAM

Posted on February 19, 2018 at 23:23Hello,I am using STM32L452 device. Is it possible to map an external SPI (not QSPI) SRAM memory as internal MCU memory before compiling using the linker? I was thinking about such memory: http://www.microchip.com/...

Resolved! STM32F051 TIM2 counting way too fast?

Posted on February 20, 2018 at 10:27I'm trying to use TIM2 on the STM32F0-Discovery board (I am new to the STM32, but have used the STM8 before).I setup TIM2 and USART1, then in a loop I send the value of TIM2_CNT via the USART1, so I can see how TI...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.