2026-06-02 6:14 AM - last edited on 2026-06-03 2:12 AM by Andrew Neil
Title edited to clarify that this is about using the STLINK-V3SET with & without the B-STLINK-ISOL adapter board.
hi ,
is there a easiest way to shift the STLINK v3 from ISOL to normal , during debugging it is ok with ISOL as the device has power.
but if i want to just use as a programmer without external power, then i have to remove the isol board and put back the jumpers .
is there a easiest way
2026-06-02 7:01 AM
Just to be clear, you're talking about the STLINK-V3SET with B-STLINK-ISOL adapter board - yes ?
2026-06-03 1:44 AM
Yes
2026-06-03 5:32 AM
The simplest solution could be to get a second STLINK-V3SET, which you can use as an alternative without any modification and without a B-STLINK-ISOL.
Regards
/Peter
2026-06-03 5:54 AM - edited 2026-06-03 5:54 AM
@prudhvichitturi or, perhaps, get one of the cheaper STLink V3 variants for when you don't need the isolation and/or the V3SET's other extra features ... ?
eg,
Or even the good ol' ST-LINK/V2
2026-06-05 4:53 AM
thank you
I do have STLINK-V2 , but i was wondering if there is a way to use STLINK v3 with out changing the programmers for the programming and debugging- vice versa.
2026-06-05 4:55 AM
looks like there once its isol , wondering if there is a jumper will do :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.