2022-02-01 10:43 PM
hello , I use spi and ı use slave mod spi. When I send a frequency of 500khz or more as a clock so data is shifting or I recieve wrong data but I send a frequency less than 500 khz I recieve true data. what is the reason of this.( use stm32h743zı)
2022-02-02 12:06 AM
Hook up a logic analyzer, even a cheap USB one or better a scope and check the timing/waveforms. Maybe the waveforms are bad and the timing works only for lower clocks. Or the sampling point (SPI mode) is wrong. Do you handle a SS/CS pin? Maybe that handling is too slow.
hth
KnarfB
2022-02-02 12:14 AM
I dont use cs/ss pin and ı check waveforms no problem appears,
2022-02-02 12:19 AM
> recieve wrong data
are bits flipped or shifted? Always the same pattern or random? Can you force specific bit patterns (0xFF, 0x55, 0xAA,...) for better testing?
2022-02-02 12:31 AM
for example I send 0xC1BA(1100 0001 1011 1010) and I check pin with oscilloscope I see 0x8375(1000 0011 1011 0101), data is 1 bit shift left but if frequency is less than 500 khz no problem.
2022-02-02 2:54 PM
Sounds like slave is not ready to receive when the master sends the first bit. And/or incorrect CPHA/CPOL settings.
> ı check waveforms no problem appears,
Show them. The problem is somewhere and it's unlikely to be an STM32 hardware issue. Show relevant code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.