2022-02-02 1:17 PM
This is the how I'm trying to write to flash
Basically I pass my uint16_t array to a function called FLASH_WriteA which accepts the array, the destination array or the location and the length
void FLASH_WriteA(uint16_t * src, uint16_t * dest, uint16_t length_16)
{
uint32_t firstAddress= FLASH_GetFirstAddress((uint32_t)dest, PAGE_SIZE_BYTES); // gets the first address of that page
uint32_t offset = ((uint32_t)dest - seg) / 2; // offset is in words
HAL_FLASH_Unlock();
Flash_Erase_Page((uint16_t*)seg); // calls the page erase function
FLASH_Write_HAL((uint32_t *)&flashBuffer, (uint16_t*)seg, FLASH_TABLE_SIZE_BYTES); //FLASH_TABLE_SIZE_BYTES = 256 = size of array
HAL_FLASH_Lock();
}
HAL_StatusTypeDef Flash_Erase_Page(uint16_t* seg){//, uint16_t length){
//uint16_t pages = (length/page_size) + (int)((length % page_size) != 0);
uint32_t pages = 2; // page size for STM32L053 = 128 bytes
FLASH_EraseInitTypeDef EraseInitStruct;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.PageAddress = seg;
EraseInitStruct.NbPages = pages;
uint32_t PageError;
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK) //Erase the Page Before a Write Operation
{
return HAL_ERROR;
}
}
void FLASH_Write_HAL(uint32_t *p_source, uint16_t* seg, uint16_t length)
{
uint32_t varToPass;
uint16_t wordcount=0;
int i;
for (i=0; i<length; i++){
varToPass = p_source[i] ;
HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD,seg+wordcount,varToPass);
wordcount += 4;
// if (wordcount>=256){
// break;
// }
}
}
2022-02-02 2:03 PM
seg isn't defined as a parameter in the function that you use it in, while src is never used.
You don't show the values you're passing to FLASH_WriteA, so who knows.
Perhaps you're trying to erase pages the program resides in.
2022-02-02 2:21 PM
seg basically gets the starting address of the fourth last page. I have debugged this.
The error during debugging actually occurs during the HAL_FLASH_PROGRAM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.