STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 ADC does not stop

Hello,According to the Reference Manual of the STM32L431 controller, the ADSTP in the ADC_CR register must be set to 1 to stop the ADC. Additional condition is that both ADSTART=1 and ADDIS=0 must be. Once the ADC is stopped, the ADSTP bit is cleared...

user 143 by Associate III
  • 1812 Views
  • 2 replies
  • 0 kudos

SPİ SCK frequency ?

hello , I use spi and ı use slave mod spi. When I send a frequency of 500khz or more as a clock so data is shifting or I recieve wrong data but I send a frequency less than 500 khz I recieve true data. what is the reason of this.( use stm32h743z...

Writing to array to flash memory which is uint16_t. I am using a STM32L053 nucleo. My program gets a hard fault error.

This is the how I'm trying to write to flashBasically I pass my uint16_t array to a function called FLASH_WriteA which accepts the array, the destination array or the location and the lengthvoid FLASH_WriteA(uint16_t * src, uint16_t * dest, uint16_t ...

AV.9 by Associate II
  • 1876 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4R: How do Flash Option DBANK and DB1M interacts?

In FLASH_OPTR, both DBANK and DB1M are r/w and have no restrictions beside that PCROPA/B needs to be disabled. For 1M device there are two(?) sensible settings DBANK=1, DB1M = 1 for 1Myte dual bank continous modeDBANK=0, DB1M = 0 for 1Myte single ban...

Implement Cordic of Arctan2 through ADC and DMA

I need to calculate angle value with input of sin/cos from ADC1/ADC2 channel by DMA way. As using the cordic of atan2 function,I think that two parameters of Y and X need to be written to pInBuff as like the key code below, is it correct? sCordicConf...

CWang.9 by Associate
  • 1164 Views
  • 0 replies
  • 0 kudos

Is five-volt tolerance guaranteed in Standby / Stop mode?

I want to wake-up from standby mode on a STM32L422xx using PA2 (WKUP4) with pull-down enabled in PWR_PDCRA. Wake-up signal can go up to 5.25V at this pin.Can this configuration cause any problems e.g. high current injection during wake-up phase?Thank...

C.Ecke by Associate
  • 831 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.