2021-03-24 4:34 AM
I would like to advise you, I create software for the STM32L151C8 microcontroller that will control the LCD segment display via the I2C PCF85176 driver
Design:
- battery powered
- configurable by the attached bluetooth module and keeping configuration values in EEPROM / FLASH
- pulse ounter on the interrupt and holding the value in the flash, the device does not reset after inserting the battery
- displaying on LCD pulse values after simple mathematical operations (addition, multiplication)
My questions:
void LCD_Update(void) {
uint8_t msg[2+20];
uint8_t *display_mem=msg+2;
msg[0]=CMD_OPCODE_DEVICE_SELECT | 0 | CMD_CONTINUE;
msg[1]=CMD_OPCODE_LOAD_DATA_POINTER | 0;
memset(display_mem, 0, 20);
int i,j;
for(i=0;i<8;i++) {
for(j=0;j<4;j++) {
uint8_t nibble=(display_digits[i]>>(4*j))&0xf;
uint8_t nibbleaddr=digit_addrs[i][j];
uint8_t byteaddr=nibbleaddr>>1;
nibbleaddr&=1;
display_mem[byteaddr]|=nibble<<(4*nibbleaddr);
}
}
HAL_I2C_Master_Transmit(&hi2c1, PCF8576_ADDR, msg, sizeof(msg), 100);
}
void LCD_Clear(void) {
for(int i=0;i<=8;i++) {
display_digits[i]=0;
}
LCD_Update();
}
void LCD_Print(char* str) {
int idx=0;
for(int i=0;i<=8;i++) {
char c=str[i];
if(c>='A' && c<='Z') {
display_digits[idx]=alpha[c-'A'];
}
else if (c=='.') {
display_digits[idx-1]=numsDot[str[i-1]-'0'];
idx--;
}
else if(c>='0' && c<='9') {
display_digits[idx]=nums[c-'0'];
}
idx++;
}
LCD_Update();
}
void LCD_PrintInt(int value) {
char str[8];
sprintf(str, "%d", value);
LCD_Print(str);
}
void LCD_PrintFloat(float value, uint8_t length) {
char str[length];
snprintf(str, length + 1, "%f", value);
LCD_Print(str);
}Above is fragment of my program to control LCD
2021-03-24 6:06 AM
> I choose good MCU for this application?
That depends on your application.
If the MCU can fulfill the timing requirements, and your application fits in the Flash space, you are fine.
> using the snprintf / sprintf function to convert floats to char array - it uses a lot of memory?
> using float (this MCU don't have FPU i should using uint and only add dot on LCD?)
The toolchain will add emulation code if necessary, increasing code size.
A FPU does help very little for printf-like functions.
Most CPU-intensive calculation routines can be implemented with integer, which is usually faster than FPU-based calculations.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.