STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I use a STM32L151 in a battery application, i have to measure VCC. To do this exactly i try to read the Vrefint-calibration Value, stored at 0x1ff80078/9 (STM32L151 Datasheet pg. 56) But if i try to access to this address via a pointer, i read 0x0.

Memory Dump with STM32CubeIDE shows also 0x0 at this addess. The Errata shows no entry to this problem.uint32_t* ptr = 0x1FF80078;VREFINT_CAL_VAL = *ptr;Is it a typo in the dataheet?

SGass.1 by Associate
  • 1994 Views
  • 3 replies
  • 0 kudos

Some questions about using float, snprintf, sprtinf

I would like to advise you, I create software for the STM32L151C8 microcontroller that will control the LCD segment display via the I2C PCF85176 driverDesign:- battery powered- configurable by the attached bluetooth module and keeping configuration v...

ughr1 by Associate II
  • 1295 Views
  • 1 replies
  • 0 kudos

What is Actually ADC sampling rate. Suppose i want to trigger the adc at sampling rate of 1Msps. i would trigger the adc using timer update event that would over flow after every 1 usec. But in the parameter setting using cube mx for adc has one option

of sampling time in terms of cycles. what this sampling time corresponds to. I mean is this the actual rate at which the adc samples the input signal. If this is Sampling rate of ADC. then using Timer update event which i set for every 1hmz is relate...

The SWD and Trace ports on STM32H7

The SWD port appears to be dedicated to CM7 core. My first question is whether it can be dedicated to CM4 and second question is how to use Trace port on CM4?Thanks

RBharol by Associate III
  • 2021 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.