2020-12-10 10:00 PM
I am planning to interface 4 numbers of Wiz830MJ modules with STM32L496 using FMC SRAM interface. Is there a need to have buffers for address bus and transceivers for data bus. OR else Can i manage without these buffers/tranceivers ?
2020-12-10 11:25 PM
I don't know what exactly the modules are (I am not going to look up their datasheet etc.), but generally, the GPIO "speeds" figure in the STM32 datasheets are given with a 50pF load; and I guess 4 chips' load is roughly in that range, so unless there's more that just one chip on the module, from that point of view it should be OK.
JW
2020-12-11 12:07 AM
Thanks for your reply. You need not look into the datasheet. My concern is can I connect 4 standard SRAMs to STM32 via FMC interface. While doing so the address bus, data bus, OE & WR signals will be shared among all. As a good practice and also for avoiding loading the buffers & transceivers are used in general for the older designs. I just want to know whether STM32 latest products like STM32L496 can work with such loads.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.