STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STML433RC (nucleo kit) LPUART1 not working

Hello,I have generated a default project with cubeIDE for a nucleo L433RC. I have only enabled LPUART1 with default parameters. I just change the baud rate to 115200.I add in the main : /* Infinite loop */   /* USER CODE BEGIN WHILE */   char out[6...

0693W000006FRE4QAO.png
PBoym.1 by Associate II
  • 1618 Views
  • 2 replies
  • 0 kudos

I use the core STM32G431KBT6 the 10v power supply via Vin I want to monitor a variable via STm Studio, but when I insert the USB into the pc the variables are reset

hi, Reading the UM2397 manual on page 12 chapter "Power supply" describes the possibility of powering the core through Vin in a voltage range of 7V-12V, I power it at 10v (the power supply can supply 500mA sufficient current for a core). The card the...

Mbert.1 by Associate II
  • 2730 Views
  • 2 replies
  • 0 kudos

IAP project ,fail to jump to application

the atteched file mbxfirmware_ebike is our solution code . we have three projects .and I am doing the bootloader testing . ​the mbxEbike is my application project ,and I set #define VECT_TAB_OFFSET 0x8000 /*!< Vector Table base offset field.in this...

0693W000006F79EQAS.png
slu.7 by Associate II
  • 1236 Views
  • 1 replies
  • 0 kudos

USB C Power Role swap by STUSB1600

Hi ,We are making one android accessory which required to pass through power support from accessory to android smartphone.Now we also want to communicate with smartphone by keeping our accessory in device mode.So by using STUSB1600 , Can I do data / ...

PVala.1 by Associate II
  • 2262 Views
  • 3 replies
  • 0 kudos

Generate velocity curve

Hi, I am a NUCLEO STM32H743ZI2 and I am trying generate one velocity curve with the register ARR. I'm using 3 stepper motors and firstly I tested the code with constant velocity but when I increment the velocity from 0 rpm to 2 rpm by 0.001 and the s...

SRivi.1 by Associate II
  • 1089 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.