2020-09-11 1:14 AM
Hi everyone
I'm working with Sim800 which is a module for many applications such as in my case, sending and receiving SMSs. in my code, I send a certain text to Sim800 in SMS form and then I send an AT command to read it. now I want to analyze this received message. I've stored the received messages in a 250elements array called
char Rcv[250];this is the code in which I analyze my Rcv[]
this part is declared in my code before main()
char Rcv[250], USERS[10][13];
char CODENUMBER[36]="06A9062F0020063406450627063106470020";
int inc=0,click=0;and this part is in while()
for(int i=0;i<250;i++)
{
if(Rcv[i]=='0' && Rcv[i+1]=='6' && Rcv[i+2]=='A' && Rcv[i+3]=='9' && Rcv[i+4]=='0' && Rcv[i+5]=='6' && Rcv[i+6]=='2' && Rcv[i+7]=='F' && Rcv[i+12]=='0' && Rcv[i+13]=='6' && Rcv[i+14]=='3' && Rcv[i+15]=='4' && click==0) //Check if "CODE SH" is sent
{
click=1;
TextMode();
DeleteSMS();
HAL_Delay(2000);
for(int i=0;i<250;i++)
{
while(Rcv[i]==CODENUMBER[inc] && inc<36)
{
inc++;
if(inc==36)
{
for(int j=0;j<10;j++)
{
if(USERS[j][0]=='\0')
{
HAL_Delay(1000);
for(int n=0;n<12;n++)
{
USERS[j][0]='+';
USERS[j][n+1]=Rcv[i+8+4*n];
}
HAL_Delay(1000);
AddPrompt(USERS[j]);
HAL_Delay(3000);
j=10;
ClearRcv(); // to set each element of Rcv[]='\0'
i=250;
inc=0;
}
}
ClearRcv(); // to set each element of Rcv[]='\0'
}
}
}
click=0;
}
}
}so I first check if I got the CODENUMBER text(which is a unicode message) right, and then I check if the USERS[10][13] array has any empty row to fill it with certain "char"s that I search within Rcv[] .
the problem is that even though I clear Rcv[] each time, next time it wouldn't be filled from it's 0th element! and I can see my message is started some where in the middle or at the end of Rcv[]! and rest of it is placed from 0th element! I don't know why this happens and this makes it impossible to analyse the message since I should receive CODENUMBER in a way that Rcv[i] and Rcv[i+1] ect. are continuously after each other and not in a way that one of them is placed at the bottom of Rcv[](say Rcv[250]) and the next one is placed in Rcv[0]!
any help guys?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.