2026-02-03 4:29 AM
Dear all
I am using STM32H563 and interface with some CAN bus sensors to receive and sometimes send data to them. The CAN bus sensors are developed by a partner company. I developed my software refer to FDCAN_Com_IT example provided in IDE firmware package. They work fine most of time, but there is an issue has been bother me - for a few sensors, tmy software doesn't receive the message form them, it doesn't generate interrupt simply. Don't think the sensor module is fault as they can be received by a CANUSB dongle, it seems the issues are with a few fixed sensor modules only, so i am wonder what I have done wrong to miss the message, on Logic analyser, message can be seen although sometimes it is with error, but most of time, they are fine, just doesn't reach my ISR.
Regards!
Ping
Solved! Go to Solution.
2026-02-03 8:58 AM
Try:
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0U;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0;
sFilterConfig.FilterID2 = 0;
2026-02-03 4:53 AM
You would need to present that FDCAN configuration settings (code) to check this issue.
Perhaps the message filtering settings are the problem.
Set those to default (no filtering), and implement filters later, once communication works otherwise.
Additionally I would check the TEC and REC fields in the CAN status.
2026-02-03 5:09 AM
And maybe the messages that you can't receive use bit rate switching (BRS) ?
2026-02-03 5:23 AM
Hi, LCE, thanks for reply!
Below is FDCAN configuration - CAN sensor use extended message ID at 500kbps, they are all same.
hfdcan2.Instance = FDCAN2;
hfdcan2.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan2.Init.AutoRetransmission = ENABLE;
hfdcan2.Init.TransmitPause = ENABLE;
hfdcan2.Init.ProtocolException = ENABLE;
hfdcan2.Init.NominalPrescaler = 4;
hfdcan2.Init.NominalSyncJumpWidth = 1;
hfdcan2.Init.NominalTimeSeg1 = 70;
hfdcan2.Init.NominalTimeSeg2 = 54;
hfdcan2.Init.DataPrescaler = 1;
hfdcan2.Init.DataSyncJumpWidth = 1;
hfdcan2.Init.DataTimeSeg1 = 1;
hfdcan2.Init.DataTimeSeg2 = 1;
hfdcan2.Init.StdFiltersNbr = 1;
hfdcan2.Init.ExtFiltersNbr = 1;
hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK)
{
Error_Handler();
}Below is the code snap for filter configuration, it accept all message IDs, basically.
/* USER CODE BEGIN FDCAN2_Init 2 */
/* Configure standard ID reception filter to Rx FIFO 0. accept any message IDs */
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_EXTENDED_ID;
sFilterConfig.FilterIndex = 0U;
sFilterConfig.FilterType = FDCAN_FILTER_RANGE_NO_EIDM;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x00000000;
sFilterConfig.FilterID2 = 0x1FFFFFFF;
if (HAL_FDCAN_ConfigFilter(&hfdcan2, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
/**
* Configure global filter:
* - Filter all remote frames with STD and EXT ID
* - Reject non matching frames with STD ID and EXT ID
*/
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan2,
FDCAN_REJECT, FDCAN_REJECT,
FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
/* Activate Rx FIFO 0 new message notification */
if (HAL_FDCAN_ActivateNotification(&hfdcan2, (FDCAN_IT_RX_FIFO0_NEW_MESSAGE | FDCAN_IT_RX_FIFO0_FULL), 0U) != HAL_OK) //enable interrupt
{
Error_Handler();
}
/*##-2 Start FDCAN controller (continuous listening CAN bus) ##############*/
if (HAL_FDCAN_Start(&hfdcan2) != HAL_OK)
{
Error_Handler();
}I did check BRS from received message , it doesn't use BRS, all sensor modules are programmed with same code.
Regards!
Ping
2026-02-03 5:29 AM
Hello,
@Ping1 wrote:
for a few sensors, tmy software doesn't receive the message form them, it doesn't generate interrupt simply.
1 - Are these sensors (not working) are same as the others which are working? bitrate issue? connection issue?
You need to sniff the frames at CAN_H/CAN_L of the sensors to confirm the sent frames from STM32H5 are well seen on CAN pins of these sensors.
2- It could be also a filtering issue. But for that you need to be sure of:
- The frames are well seen on CAN_H/CAN_L
- The bitrate used by these sensors is the same of what you have configured in STM32H5.
2026-02-03 5:31 AM - edited 2026-02-03 5:34 AM
You didn't show the code responsible of sending frames to the sensors.
Also try the filter config:
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0U;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0;
sFilterConfig.FilterID2 = 0;
2026-02-03 6:50 AM
Hi, mƎALLEm
Thanks for response!
The ISR code is shown below, as you can see, I am counting 3 messages from 3 different sensors with different message IDs.
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
if ((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != 0U)
{
/* Retrieve Rx messages from RX FIFO0 */
if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &rxHeader, rxData) != HAL_OK)
{
Error_Handler();
}
if(rxHeader.Identifier == 0x1f000017) {
rxed2++;
}
if(rxHeader.Identifier == 0x1f00001A) {
rxed3++;
}
if(rxHeader.Identifier == 0x1f000024) {
rxed6++;
}
memcpy(&rxCopy, &rxData, 8);
tx_semaphore_put(&semaphore_can); //received a message
}
}Below is the sending message thread: after it receives different type so message, for now reply with an initial TYPE_CONFIG_REQUEST message, and then for all TYPE_OCC_DATA message, I just sent it on bus for test only.
VOID FDCAN_thread_entry(ULONG initial_input)
{
ULONG current_value;
TX_THREAD *first_suspended;
ULONG suspended_count;
TX_SEMAPHORE *next_semaphore;
HAL_StatusTypeDef sendStatus;
//uint8_t rxed = 0;
FDCAN_TxHeaderTypeDef txHeader;
while(1) {
can_TS = HAL_GPIO_ReadPin(FDCAN_TS_GPIO_Port, FDCAN_TS_Pin); //SET means it is in normal mode,
/* Check one message is received in Rx FIFO 0 */
tx_semaphore_get(&semaphore_can, TX_WAIT_FOREVER);
UINT status = _tx_semaphore_info_get(&semaphore_can, NULL, ¤t_value, &first_suspended, &suspended_count, &next_semaphore);
if(status == TX_SUCCESS) {
//send a reply message with what rxed content ID and data
if(rxData[7] == TYPE_CONFIG_REQUEST) {
txData[0] = 0x01; //enable indicator
txData[5] = 0x64; //0.2s, 0x64~1s, 0xC8 data packet every 2s for now
txData[7] = TYPE_CONFIG_REPLY;
txHeader.Identifier = rxHeader.Identifier - 0x1f000000;//unicast one // //broadcast to all
txHeader.IdType = FDCAN_EXTENDED_ID;
txHeader.TxFrameType = FDCAN_DATA_FRAME;
txHeader.DataLength = FDCAN_DLC_BYTES_8;
txHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
txHeader.BitRateSwitch = FDCAN_BRS_OFF;
txHeader.FDFormat = FDCAN_CLASSIC_CAN; //classic works, FD works too
txHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;
txHeader.MessageMarker = 0x11U;
sendStatus = HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan2, &txHeader, txData);
if(sendStatus != HAL_OK)
{
FDCAN_Error_Handler();
}
}
else if(rxData[7] == TYPE_OCC_DATA){
rxedCnt++;
/* this is for test only - send out a can msg to confirm we received it */
txHeader.Identifier = rxHeader.Identifier + 0x800000; //rxHeader.Identifier means send from Mother board 0x1f800005 for test
txHeader.IdType = FDCAN_EXTENDED_ID;
txHeader.TxFrameType = FDCAN_DATA_FRAME;
txHeader.DataLength = FDCAN_DLC_BYTES_8;
txHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
txHeader.BitRateSwitch = FDCAN_BRS_OFF;
txHeader.FDFormat = FDCAN_CLASSIC_CAN; //classic works, FD works too
txHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;
txHeader.MessageMarker = 0x12U;
sendStatus = HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan2, &txHeader, rxCopy);
if(sendStatus != HAL_OK)
{
FDCAN_Error_Handler();
}
}
}
tx_thread_sleep(10);
}
}Also, tried your filter config, no difference, BTW, I am using extended message ID, that is the only change from your suggestion.
Thank for your attention.
Ping
2026-02-03 6:54 AM
Hi, regarding
"You need to sniff the frames at CAN_H/CAN_L of the sensors to confirm the sent frames from STM32H5 are well seen on CAN pins of these sensors."
I am not sure how to sniff CAN_H/CAN_L, I am only sniff CAN_RX and CAN_TX between MCU and CAN Transceiver. Sometime, RX pins with message errors, sometimes not, but in ant case, I don't get it from my ISR, while it works for other 2 on same bus.
Regards!
Ping
2026-02-03 7:27 AM
Filter:
Just to make sure it's not the filter, comment out the call to HAL_FDCAN_ConfigGlobalFilter() or change it from FDCAN_REJECT to FDCAN_ACCEPT_IN_RX_FIFO0 or FDCAN_ACCEPT_IN_RX_FIFO1 .
Surely only if you have set up the according RX FIFO...
2026-02-03 7:52 AM
Hi, ICE
Thank you for reply.
Tried first to remove it and seems no difference made, then tried to change to below - i am receiving extended ID only.
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_EXTENDED_ID;
sFilterConfig.FilterIndex = 0U;
sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x00000000;
sFilterConfig.FilterID2 = 0x1FFFFFFF;
if (HAL_FDCAN_ConfigFilter(&hfdcan2, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan2,
FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_ACCEPT_IN_RX_FIFO0,
FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}Still makes no difference, I hope I made the change correct, let me know if i misunderstand anything.
Thank you!
Ping
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.