STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F030R8T6 ADC Calibration Error

i am using Nucleo-F030R8 board. I want to get adc calibration factor.By writing #define VREFINT_CAL (*((uint16_t *) 0x1FFFF7BA))i got VREFINT_CAL = 1521 which is actually factory stored value, that good no problem.but when i try to calibrate it by...

sanju by Senior
  • 1560 Views
  • 6 replies
  • 0 kudos

Resolved! How to change Synchronous Pre-Divider

I am using an F4 discovery board and trying to using the included 8MHz HSE crystal to drive the RTC. I am using CubeMX to configure everything and I have configured the RTC to generate the calibration 1Hz signal that I am watching on a scope. Initial...

JScri.1 by Associate
  • 3770 Views
  • 2 replies
  • 1 kudos

Resolved! 3 Phase sine wave generation

Hi all, i am trying to generate a 3 phase sine wave with 120 degree phase shift by using stm32f030r8t6 nucleo board. i can see the generated 3 phase sine wave on oscilloscope but the freq is not stable of the sine wave. it varies continuously from 40...

sanju by Senior
  • 11193 Views
  • 15 replies
  • 0 kudos

How to manage write pointer of FMAC?

Hi all,imagine I want to implement two FIR filters (for I and Q, that is very common task for signal processing). First I set X1 buffer to 0 and size, let say, 32, and push there let say four data, thus write pointer is 4. Then I set X1 buffer to 32 ...

DmRozhd by Associate III
  • 922 Views
  • 0 replies
  • 1 kudos

Receiving Messages from Sim800

Hi everyoneI'm working with Sim800 which is a module for many applications such as in my case, sending and receiving SMSs. in my code, I send a certain text to Sim800 in SMS form and then I send an AT command to read it. now I want to analyze this re...

Ala by Senior
  • 1191 Views
  • 0 replies
  • 0 kudos

Resolved! RAM function (code) placement using GNU GCC family

Hi guys,I would like to ask how properly place the function (code). I have solved the ld. script (have already the section in ram for code there) and functions which I want to place in ram has section attributes, but I read that the long call attribu...

binarybee by Associate III
  • 4387 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.