2018-07-11 6:24 AM
Hello,
I am using the SPWF01SA incorporated into a board with a microcontroller that is responsible for responding to orders that come through the module.
My problem is that through the page ''output_demo.html'' I can send messages without problem, but I have no option to view the messages I receive from the board. The ''input_demo.shtml'' page always shows me the following message:Since I have this error, to see the messages sent from the board I open a socket with the command AT + SOCKD = 32000 and access it through the SocketTest program. So far everything is correct, but when I add the network to a local network with an internet connection, this socket disappears.
Is there any chance that when I add the network to another one, this socket it will remain open and I will be able to communicate through it?
Thanks
#spwf01sa #socket #wifi-sp*We’re moving the ST Community to a new platform to give you a better and more reliable community experience.