2023-10-07 4:49 AM
Hello,
i am having problems to read data from the QSPI nor-flash if the address changes from 0x90FFFFFF to 0x91000000
Everything is fine from 0x90000000 to 0x90FFFFFF but beginning from 0x91000000 there is no data.
Example, i have an array stored at the qspi which is stored in 0x90 and it goes into the 0x91 address.
i try to copy the array to a local array which does not work. When i debug, i see that at 0x91000000 seems to be empty. Attached Screenshot 1
If read the with CubeProgrammer, and start from 0x90FFFF00 i see data but it also stops at 0x91000000
Attached Screenshot 2
But, when starting reading from 0x91000000 i see the data correctly.
Attached Screenshot 3
I am using a custom PCB, STM32F779, MX25L512 QSPI with touchgfx
The arrays at the qspi i want to have access are only for reading, i don't want to write to the qspi.
What is my problem here? How can i get access to the address over 0x90FFFFFF ?
Thanks for any help.
Solved! Go to Solution.
2023-10-07 5:51 AM
The parts default into 3-byte / 24-bit addressing mode for compatibility purposes. The 3-byte addressing mode works for devices of 16MB (128Mbit) or smaller
You need to command them into 4-byte / 32-bit addressing mode, or use secondary commands identifying as being 4-byte address ones.
At the hqspi structure level this is a STM32 QSPI Peripheral directive as how to deliver the address, the flash chip needs to be in mode to accept that.
2023-10-07 5:05 AM
As presented it suggests an issue with the External Loader implementation.
At 16MB might suggest incorrect handling of 24 / 32-bit addressing modes or commands.
Are you sure this isn't mirroring content at 0x90000000 ?
2023-10-07 5:24 AM
Thank you very much for your answer and for the very helpful tip regarding the external loader and bit addressing.
I just checked my custom external loader and indeed i use 24 bit there
uint8_t CSP_QSPI_Erase_Chip(void) {
QSPI_CommandTypeDef sCommand;
if (QSPI_WriteEnable() != HAL_OK) {
return HAL_ERROR;
}
/* Erasing Sequence --------------------------------- */
sCommand.Instruction = CHIP_ERASE_CMD;
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.AddressSize = QSPI_ADDRESS_24_BITS;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
sCommand.AddressMode = QSPI_ADDRESS_NONE;
sCommand.Address = 0;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
That means that i need 32 bit if i use more than 16MB, right?
At my main program i use:
s_command.AddressSize = QSPI_ADDRESS_32_BITS;That might be a reason why my custom bootloader loads the data to the correct address but the external loader used in cubeIDE and CubeProgrammer can not read the data correctly.
I will give it a try to change the bit from 24 to 32 at the custom loader.
2023-10-07 5:51 AM
The parts default into 3-byte / 24-bit addressing mode for compatibility purposes. The 3-byte addressing mode works for devices of 16MB (128Mbit) or smaller
You need to command them into 4-byte / 32-bit addressing mode, or use secondary commands identifying as being 4-byte address ones.
At the hqspi structure level this is a STM32 QSPI Peripheral directive as how to deliver the address, the flash chip needs to be in mode to accept that.
2023-10-07 6:01 AM
2023-10-07 6:58 AM
2023-10-07 9:33 AM
Thank you so much.
It works now, and i can put my custom arrays to the end of the qspi, that was never working.
The problem i had when i used the qspi up 16MB that the graphics are destroyed is also gone now. Thanks so much.
I also saw that your sector size is different to my initial external loader (which worked for the first 16MB).
I now need to find out where the problem is, i can not upload from cubeIDE
Error: failed to erase memoryBut on cubeProgrammer it works.
I will try to find out where the problem at my external loader is for better understanding in the future.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.