cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Touchgfx "Program and Run Target" ->STM32N6570-DK

MEige
Associate II

Hello

"Program and Run Target" stops with some Messages (Small Test Prog.)

"Program All":

              -------------------------------------------------------------------
                               STM32CubeProgrammer v2.22.0                  
              -------------------------------------------------------------------

        Memory Programming ...
          File          : STM32N6570-DK_FSBL-trusted.bin
          Size          : 32.63 KB 
          Address       : 0x70000000       
        
        Erasing memory corresponding to segment 0:
        Erasing external memory sector 0
        Error: failed to erase memory
        
        Error: failed to erase memory
        c:/TouchGFXProjects/MyApplication_5/gcc/include/flash_sections_int_ext.mk:18: recipe for target '_fsblflash_' failed
        make[2]: *** [_fsblflash_] Error 1
        makefile_fsbl:45: recipe for target 'flash' failed
        make[1]: *** [flash] Error 2
        ../../gcc/Makefile:8: recipe for target 'flash' failed
        make: *** [flash] Error 2
        Failed

 

"Program Internal Flash":

        Memory Programming ...
          File          : STM32N6570-DK_Appli-trusted.bin
          Size          : 345.22 KB 
          Address       : 0x70100000     
        
        Erasing memory corresponding to segment 0:
        Erasing external memory sectors [16 21]
        Error: failed to erase memory       
        
        Error: failed to erase memory
        c:/TouchGFXProjects/MyApplication_5/gcc/include/flash_sections_int_ext.mk:12: recipe for target '_intflash_' failed
        make[2]: *** [_intflash_] Error 1
        makefile_appli:55: recipe for target 'intflash' failed
        make[1]: *** [intflash] Error 2
        ../../gcc/Makefile:12: recipe for target 'intflash' failed
        make: *** [intflash] Error 2
        Failed
    Failed

 

A second "Program and Run Target"  is necessary to correctly programm the STM32N6. To start the Prog.  a Cold Boot (Power off/of) is necessary.

PC: Standard PC Win 10

BTW: Some Demos are making Problems also. The "Coffee Machine Demo" stops with

 

     make (e=206): Der Dateiname oder die Erweiterung ist zu lang.
        
        make[3]: *** [Appli/TouchGFX/build/bin/target.elf] Error 206
        make[2]: *** [generate_assets] Error 2
        Failed
        ../../gcc/Makefile:8: recipe for target 'all' failed
        make[1]: *** [all] Error 2
        make: *** [all] Error 2
    Failed

Der Dateiname oder die Erweiterung ist zu lang = Filename or Extension is to long.

Marc

1 ACCEPTED SOLUTION

Accepted Solutions
MEige
Associate II

Edit:

I managed to get the Coffee demo running. I changed OS from FreeRTOS to ThreadX.

View solution in original post

1 REPLY 1
MEige
Associate II

Edit:

I managed to get the Coffee demo running. I changed OS from FreeRTOS to ThreadX.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.