cancel
Showing results for 
Search instead for 
Did you mean: 

Porblem with IS66WVH64M8DBLL-166B1LI and STM32H723VGT6

DMast.1
Associate II

Good morning,

I'm writing because we are spending a lot of time in the last weeks due experiencing a problem accessing the 64MByte external RAM (IS66WVH64M8DBLL-166B1LI) via Hyperbus on our target board. If we replace the ISSI memory with a Cypress/Infineon, we can access the memory in bytes, words, or dwords with no problem. To exclude layout issues on our board, we purchased the STM32H735G-DK evb and, after verifying that everything worked correctly with the original memory, we replaced it with the 64MByte ISSI and the same problems we're having with our board appear. Specifically, accessing bytes at even addresses results in no errors, while trying to write and re-read bytes at odd addresses results in significant errors. The situation doen's change even if we let's slow down with clock (20MHz). 

Here is the device init code

/* Initialize OctoSPI ----------------------------------------------------- */
OSPIHandle.Instance = OCTOSPI2;
HAL_OSPI_DeInit(&OSPIHandle);

OSPIHandle.Init.FifoThreshold = 4;
OSPIHandle.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
OSPIHandle.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;

OSPIHandle.Init.DeviceSize = POSITION_VAL(OSPI_RAM_SIZE);

OSPIHandle.Init.ChipSelectHighTime = 4;//>> 2;
OSPIHandle.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
OSPIHandle.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
OSPIHandle.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
OSPIHandle.Init.ClockPrescaler = 2;//>> 4;
OSPIHandle.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
OSPIHandle.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;//>> HAL_OSPI_DHQC_ENABLE;
OSPIHandle.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED; //>>HAL_OSPI_DELAY_BLOCK_USED;
OSPIHandle.Init.ChipSelectBoundary = 0;
OSPIHandle.Init.MaxTran = 0;
OSPIHandle.Init.Refresh = 400;

if (HAL_OSPI_Init(&OSPIHandle) != HAL_OK)
{
Error_Handler() ;
}


/* Configure the Hyperbus to access memory space -------------------------- */
sHyperbusCfg.RWRecoveryTime = 4;//>>OSPI_HYPERRAM_RW_REC_TIME;
sHyperbusCfg.AccessTime = 6;//>>OSPI_HYPERRAM_LATENCY;
sHyperbusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;
sHyperbusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;

if (HAL_OSPI_HyperbusCfg(&OSPIHandle, &sHyperbusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}

/* Memory-mapped mode configuration --------------------------------------- */
sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
sCommand.DQSMode = HAL_OSPI_DQS_ENABLE;
sCommand.Address = 0;
sCommand.NbData = 1;

if (HAL_OSPI_HyperbusCmd(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}

sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
sMemMappedCfg.TimeOutPeriod = 0x34; /* circa 50 cicli */
if( HAL_OSPI_MemoryMapped(&OSPIHandle, &sMemMappedCfg) != HAL_OK)
{
Error_Handler();
}





And this is the memory test code:

#define DATA_OFFSET 1u

errors = 0;
mod1errors = 0;
uint8_t *pzMem = (uint8_t*) OCTOSPI2_BASE;
uint32_t total_bytes = 64u * 1024u * 1024u;

for (i = 0; i < 100; i++)
{

  for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
  {
     pzMem[zIndex] = (uint8_t) (zIndex & 0xFF);
     __asm("NOP");
  }

  for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
 {
     uint8_t read_val = pzMem[zIndex];
     uint8_t expected_val = (uint8_t) (zIndex & 0xFF);

     if (read_val != expected_val)
     {
          errors++;
     }

     __asm("NOP");
  }

}
 
 
if DATA_OFFSET is set to 2 (even byte access -> good)
if DATA_OFFSET is set to 1 (odd/even byte access -> getting errors)

Can anyone help us understand where we're going wrong and how we can get the 64MByte memory to work correctly as well? Thanks in advance

Renato

 

 

5 REPLIES 5
KDJEM.1
ST Employee

Hello @DMast.1 ;

 

Could you please check ChipSelectBoundary and Refresh values?

Chip select boundary (CSBOUND) configured depending on the memory datasheet. The chip select must go high when crossing the page boundary (2CSBOUND bytes defines the page size).
Refresh rate (REFRESH) required for PSRAMs memories. The chip select must go high each (REFRESH x OCTOSPI clock cycles), configured depending on the memory datasheet.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

As you can see in the previus code, here is the init values:

...

OSPIHandle.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;//>> HAL_OSPI_DHQC_ENABLE;
OSPIHandle.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED; //>>HAL_OSPI_DELAY_BLOCK_USED;
OSPIHandle.Init.ChipSelectBoundary = 0;
OSPIHandle.Init.MaxTran = 0;
OSPIHandle.Init.Refresh = 400;

 

..do you need something else?

KDJEM.1
ST Employee

Hello @DMast.1 ;

 

Could you please look at How to insert source code - STMicroelectronics Community to increase the readability of your content.

You need to give more details to check the parameters like as the octospi clock and share the memory datasheet. 

Also, I advise you to refer to AN5050 Table 8. STM32CubeMX - Configuration of OCTOSPI parameters and double check your configuration.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello, 

sorry but this is the first time that we use ST support.

 /* Initialize OctoSPI ----------------------------------------------------- */
  OSPIHandle.Instance = OCTOSPI2;
  HAL_OSPI_DeInit(&OSPIHandle);

  OSPIHandle.Init.FifoThreshold         = 4;
  OSPIHandle.Init.DualQuad              = HAL_OSPI_DUALQUAD_DISABLE;
  OSPIHandle.Init.MemoryType            = HAL_OSPI_MEMTYPE_HYPERBUS;

  OSPIHandle.Init.DeviceSize = POSITION_VAL(OSPI_RAM_SIZE);

  OSPIHandle.Init.ChipSelectHighTime    = 4;//>> 2;
  OSPIHandle.Init.FreeRunningClock      = HAL_OSPI_FREERUNCLK_DISABLE;
  OSPIHandle.Init.ClockMode             = HAL_OSPI_CLOCK_MODE_0;
  OSPIHandle.Init.WrapSize              = HAL_OSPI_WRAP_NOT_SUPPORTED;
  OSPIHandle.Init.ClockPrescaler        = 2;//>> 4;
  OSPIHandle.Init.SampleShifting        = HAL_OSPI_SAMPLE_SHIFTING_NONE;
  OSPIHandle.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;//>> ;
  OSPIHandle.Init.DelayBlockBypass      = HAL_OSPI_DELAY_BLOCK_USED; 

  OSPIHandle.Init.ChipSelectBoundary    = 0;
  OSPIHandle.Init.MaxTran               = 0;//>>
  OSPIHandle.Init.Refresh               = 400;//>> 0      /* vedi nota sotto */

  if (HAL_OSPI_Init(&OSPIHandle) != HAL_OK)
  {
    Error_Handler() ;
  }


  /* Configure the Hyperbus to access memory space -------------------------- */
  sHyperbusCfg.RWRecoveryTime   = 4;
  sHyperbusCfg.AccessTime       = 6;
  sHyperbusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;
  sHyperbusCfg.LatencyMode      = HAL_OSPI_FIXED_LATENCY;

  if (HAL_OSPI_HyperbusCfg(&OSPIHandle, &sHyperbusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }

  /* Memory-mapped mode configuration --------------------------------------- */
  sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
  sCommand.AddressSize  = HAL_OSPI_ADDRESS_32_BITS;
  sCommand.DQSMode      = HAL_OSPI_DQS_ENABLE;
  sCommand.Address      = 0;
  sCommand.NbData       = 1;

  if (HAL_OSPI_HyperbusCmd(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }

  sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
  sMemMappedCfg.TimeOutPeriod     = 0x34;       /* circa 50 cicli */
  if( HAL_OSPI_MemoryMapped(&OSPIHandle, &sMemMappedCfg) != HAL_OK)
  {
    Error_Handler();
  }

///MEMORY TEST CODE
#define DATA_OFFSET						1u

	errors = 0;
	mod1errors = 0;
	uint8_t *pzMem = (uint8_t*) OCTOSPI2_BASE;
	uint32_t total_bytes = 64u * 1024u * 1024u;

	for (i = 0; i < 100; i++)
	{

		for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
		{
			pzMem[zIndex] = (uint8_t) (zIndex & 0xFF);
			__asm("NOP");
		}

		for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
		{
			uint8_t read_val = pzMem[zIndex];
			uint8_t expected_val = (uint8_t) (zIndex & 0xFF);

			if (read_val != expected_val) {
				errors++;
			}

			__asm("NOP");
		}

	}

Hello,

here is the code that we are using for testing:

 /* Initialize OctoSPI ----------------------------------------------------- */
  OSPIHandle.Instance = OCTOSPI2;
  HAL_OSPI_DeInit(&OSPIHandle);

  OSPIHandle.Init.FifoThreshold         = 4;
  OSPIHandle.Init.DualQuad              = HAL_OSPI_DUALQUAD_DISABLE;
  OSPIHandle.Init.MemoryType            = HAL_OSPI_MEMTYPE_HYPERBUS;

  OSPIHandle.Init.DeviceSize = POSITION_VAL(OSPI_RAM_SIZE);

  OSPIHandle.Init.ChipSelectHighTime    = 4;//>> 2;
  OSPIHandle.Init.FreeRunningClock      = HAL_OSPI_FREERUNCLK_DISABLE;
  OSPIHandle.Init.ClockMode             = HAL_OSPI_CLOCK_MODE_0;
  OSPIHandle.Init.WrapSize              = HAL_OSPI_WRAP_NOT_SUPPORTED;
  OSPIHandle.Init.ClockPrescaler        = 2;//>> 4;
  OSPIHandle.Init.SampleShifting        = HAL_OSPI_SAMPLE_SHIFTING_NONE;
  OSPIHandle.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;//>> ;
  OSPIHandle.Init.DelayBlockBypass      = HAL_OSPI_DELAY_BLOCK_USED; 

  OSPIHandle.Init.ChipSelectBoundary    = 0;
  OSPIHandle.Init.MaxTran               = 0;//>>
  OSPIHandle.Init.Refresh               = 400;//>> 0      /* vedi nota sotto */

  if (HAL_OSPI_Init(&OSPIHandle) != HAL_OK)
  {
    Error_Handler() ;
  }


  /* Configure the Hyperbus to access memory space -------------------------- */
  sHyperbusCfg.RWRecoveryTime   = 4;
  sHyperbusCfg.AccessTime       = 6;
  sHyperbusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;
  sHyperbusCfg.LatencyMode      = HAL_OSPI_FIXED_LATENCY;

  if (HAL_OSPI_HyperbusCfg(&OSPIHandle, &sHyperbusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }

  /* Memory-mapped mode configuration --------------------------------------- */
  sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
  sCommand.AddressSize  = HAL_OSPI_ADDRESS_32_BITS;
  sCommand.DQSMode      = HAL_OSPI_DQS_ENABLE;
  sCommand.Address      = 0;
  sCommand.NbData       = 1;

  if (HAL_OSPI_HyperbusCmd(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }

  sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
  sMemMappedCfg.TimeOutPeriod     = 0x34;       /* circa 50 cicli */
  if( HAL_OSPI_MemoryMapped(&OSPIHandle, &sMemMappedCfg) != HAL_OK)
  {
    Error_Handler();
  }

///MEMORY TEST CODE
#define DATA_OFFSET						1u

	errors = 0;
	mod1errors = 0;
	uint8_t *pzMem = (uint8_t*) OCTOSPI2_BASE;
	uint32_t total_bytes = 64u * 1024u * 1024u;

	for (i = 0; i < 100; i++)
	{

		for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
		{
			pzMem[zIndex] = (uint8_t) (zIndex & 0xFF);
			__asm("NOP");
		}

		for (uint32_t zIndex = 0; zIndex < total_bytes; zIndex += DATA_OFFSET)
		{
			uint8_t read_val = pzMem[zIndex];
			uint8_t expected_val = (uint8_t) (zIndex & 0xFF);

			if (read_val != expected_val) {
				errors++;
			}

			__asm("NOP");
		}

	}

The clock speed is 100MHz, but even if we use 25Mhz the problem still remain. With cypress 8MByte hyperram all works fine even @166MHz

Attached you can find the ISSI datasheet