2012-08-13 6:05 PM
I'm looking to power the STM32F4 discovery from the micro usb port, while keeping modifications to the board at a minimum (I don't have great faith in my smd soldering).
This is my current idea:- remove r46 to ensure that the usb regulator isn't turned on by accident. - connect a diode from the PA9 pin on p2 to one of the 5V pinsAm I going to run into any problems with this setup?2012-08-14 1:48 AM
The only problem is a loss of the PA9 functionality. You don't need to remove R46 - no accident is possible due to the same rail is always present as a main power source.
2012-08-14 1:48 AM
The only problem is a loss of the PA9 functionality. You don't need to remove R46 - no accident is possible due to the same rail is always present as a main power source.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.