STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multiple software reset conditions.

Posted on September 09, 2011 at 10:35Hello,I'm developping an application with bootloader. Today I'm using USART1 to communicate with the host PC, and I'm using a software reset to enter bootloader mode on demand (bootloader check if it's a software...

root by Associate II
  • 1569 Views
  • 6 replies
  • 0 kudos

Powering STM32F4-Discovery from micro usb

Posted on August 14, 2012 at 03:05I'm looking to power the STM32F4 discovery from the micro usb port, while keeping modifications to the board at a minimum (I don't have great faith in my smd soldering).This is my current idea:- remove r46 to ensure...

devin122 by Associate
  • 1881 Views
  • 2 replies
  • 0 kudos

STM32F4DISCOVERY - PC0 and PB2 pins

Posted on August 08, 2012 at 21:30Hi,     I would like to have some more information in regard of the PC0 pin on the STM32F4Discovery. I read on the forum that quite some people use this pin as an adc channel, but on the User Manual I can see that i...

guitest02 by Associate II
  • 3105 Views
  • 3 replies
  • 0 kudos

F4 Discovery Max SPI Speed

Posted on August 11, 2012 at 02:46Hello,1. What is the maximum SPI speed I am suppose to achieve with the 8MHz HSE? 2. I would like to achieve at least 25MHz, what would it take to achieve that both code and HW? Currently with my code below I get 13...

jvaldez by Associate
  • 1504 Views
  • 2 replies
  • 0 kudos

clock problem

Posted on August 12, 2012 at 15:25I want to use the HSI, and the code is like the following: void RCC_Configuration(void) {  RCC_DeInit();  RCC_HSICmd(ENABLE);  RCC_AdjustHSICalibrationValue(0);  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2P...

614678489 by Associate II
  • 2824 Views
  • 4 replies
  • 0 kudos

STM32F0 & STM32F1 code compatibility

Posted on August 10, 2012 at 12:09Hi. I m just complete with a project using a STM8S. I went through development with a STM8S-discovery, which is by the way a great evaluation tool : cheap, and no useless peripherals such as LCD. Just had to solder ...

thibaut2 by Associate II
  • 1765 Views
  • 6 replies
  • 0 kudos

LCD Display clashes with EXTI - STM32F4 Discovery

Posted on August 13, 2012 at 11:35Good morning everyone,I managed to make my LCD Display  work by using a simple ''delay'' function which counts the time I need to wait.I also use quite a lot a interrupts in my project.The problem is: If an interrup...

I2S3_CK signal - problem with connection to stm32

Posted on October 10, 2011 at 15:27I am working on stm32f217 144pins. I try to connect signal I2S3_SCK to stm32 but all two pins (pin nr 111 and pin nr 133) which provide this connection are used by other peripherials.These pins share functionality ...

krzkrok by Associate II
  • 1513 Views
  • 2 replies
  • 0 kudos

STM32F407 CAN1 Issue

Posted on August 11, 2012 at 21:22Hi, I'm new to this forum and was wondering if someone could maybe assist me with this problem: I'm using the STM32F407IGT6 device for one of my projects. I want to use both CAN busses on the device. Currently CAN2...

schalk by Associate II
  • 2429 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.