2023-07-04 6:11 AM
Hi all,
I use STM32CubeIDE version 1.12.0 and STM32CubeMX Version: 6.8.0-RC4.
The MCU used is STM32U585
When i start my software in debug mode, some times a HardFault is detected on SysTick_Handler function.
If i use the IWDG (with compilation option named bOPTION_WITH_WATCHDOG set to 1 (see line 46 on main.c)), a HardFault is detected systematicaly on SysTick_Handler function.
If i use the sprintf instruction (compilation option named bOPTION_WITH_SPRINTF set to 1 (see line 47 on main.c)), a HardFault is detected systematicaly on SysTick_Handler function when debugger execute "sprintf(sMsg,"%3.1f",fValue);"
See all my project in attached file and a screenshot of the hardFault detected.
Thanks in advance
Christophe ALVERNHE
2023-07-04 9:33 AM - edited 2023-07-04 9:33 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.