2025-09-30 9:53 AM - last edited on 2025-09-30 9:56 AM by Andrew Neil
After solving my issue with reading the USER1 button (thanks to everyone who helped me on this forum :folded_hands:), I am now trying to handle USER1 button detection using interrupts.
My project is running in FSBL mode, so I’m using NVIC FSBL. I’m trying to configure the USER1 button (EXTI13) with a pull-down in CubeMX. …but unfortunately without success.
what is wrong ? in my configuration in CubeMX ?
Cheers
Emmanuel
my code stm32n6xx_it.c : with void EXTI13_IRQHandler(void)
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file GPIO/GPIO_IOToggle/Src/stm32n6xx_it.c
* @author MCD Application Team
* @brief Main Interrupt Service Routines.
* This file provides all exceptions handler and
* peripherals interrupt service routine.
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32n6xx_it.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */
/* USER CODE END TD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/* External variables --------------------------------------------------------*/
/* USER CODE BEGIN EV */
/* USER CODE END EV */
/******************************************************************************/
/* Cortex Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
* @brief This function handles Non maskable interrupt.
*/
void NMI_Handler(void)
{
/* USER CODE BEGIN NonMaskableInt_IRQn 0 */
/* USER CODE END NonMaskableInt_IRQn 0 */
/* USER CODE BEGIN NonMaskableInt_IRQn 1 */
/* USER CODE END NonMaskableInt_IRQn 1 */
}
/**
* @brief This function handles Hard fault interrupt.
*/
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
/* USER CODE END W1_HardFault_IRQn 0 */
}
}
/**
* @brief This function handles Memory management fault.
*/
void MemManage_Handler(void)
{
/* USER CODE BEGIN MemoryManagement_IRQn 0 */
/* USER CODE END MemoryManagement_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_MemoryManagement_IRQn 0 */
/* USER CODE END W1_MemoryManagement_IRQn 0 */
}
}
/**
* @brief This function handles Prefetch fault, memory access fault.
*/
void BusFault_Handler(void)
{
/* USER CODE BEGIN BusFault_IRQn 0 */
/* USER CODE END BusFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_BusFault_IRQn 0 */
/* USER CODE END W1_BusFault_IRQn 0 */
}
}
/**
* @brief This function handles Undefined instruction or illegal state.
*/
void UsageFault_Handler(void)
{
/* USER CODE BEGIN UsageFault_IRQn 0 */
/* USER CODE END UsageFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_UsageFault_IRQn 0 */
/* USER CODE END W1_UsageFault_IRQn 0 */
}
}
/**
* @brief This function handles Secure fault.
*/
void SecureFault_Handler(void)
{
/* USER CODE BEGIN SecureFault_IRQn 0 */
/* USER CODE END SecureFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_SecureFault_IRQn 0 */
/* USER CODE END W1_SecureFault_IRQn 0 */
}
}
/**
* @brief This function handles System service call via SWI instruction.
*/
void SVC_Handler(void)
{
/* USER CODE BEGIN SVCall_IRQn 0 */
/* USER CODE END SVCall_IRQn 0 */
/* USER CODE BEGIN SVCall_IRQn 1 */
/* USER CODE END SVCall_IRQn 1 */
}
/**
* @brief This function handles Debug monitor.
*/
void DebugMon_Handler(void)
{
/* USER CODE BEGIN DebugMonitor_IRQn 0 */
/* USER CODE END DebugMonitor_IRQn 0 */
/* USER CODE BEGIN DebugMonitor_IRQn 1 */
/* USER CODE END DebugMonitor_IRQn 1 */
}
/**
* @brief This function handles Pendable request for system service.
*/
void PendSV_Handler(void)
{
/* USER CODE BEGIN PendSV_IRQn 0 */
/* USER CODE END PendSV_IRQn 0 */
/* USER CODE BEGIN PendSV_IRQn 1 */
/* USER CODE END PendSV_IRQn 1 */
}
/**
* @brief This function handles System tick timer.
*/
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}
/******************************************************************************/
/* STM32N6xx Peripheral Interrupt Handlers */
/* Add here the Interrupt Handlers for the used peripherals. */
/* For the available peripheral interrupt handler names, */
/* please refer to the startup file (startup_stm32n6xx.s). */
/******************************************************************************/
/**
* @brief This function handles EXTI Line13 interrupt.
*/
void EXTI13_IRQHandler(void)
{
/* USER CODE BEGIN EXTI13_IRQn 0 */
/* USER CODE END EXTI13_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13);
/* USER CODE BEGIN EXTI13_IRQn 1 */
/* USER CODE END EXTI13_IRQn 1 */
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
my code main.c : with void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) to toogle my LED1
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file GPIO/GPIO_IOToggle/Src/main.c
* @author MCD Application Team
* @brief This example describes how to configure and use GPIOs through
* the STM32N6xx HAL API.
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint8_t blink = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_NVIC_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* STM32N6xx HAL library initialization:
- Systick timer is configured by default as source of time base, but user
can eventually implement his proper time base source (a general purpose
timer for example or other time source), keeping in mind that Time base
duration should be kept 1ms since PPP_TIMEOUT_VALUEs are defined and
handled in milliseconds basis.
- Set NVIC Group Priority to 4
- Low Level Initialization
*/
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* Initialize interrupts */
MX_NVIC_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
// code to test the LED1
//HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);
// HAL_Delay(1500);
//HAL_GPIO_TogglePin(LED1_GPIO_Port,LED1_Pin);
// Read the button USER1
/*
if(HAL_GPIO_ReadPin (BP1_GPIO_Port, BP1_Pin) == GPIO_PIN_RESET)
{
HAL_GPIO_TogglePin(LED1_GPIO_Port,LED1_Pin);
}
//Turn LED ON
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);
}
else
{
//Turn LED OFF
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
}
*/
}
/* USER CODE END 3 */
}
/* USER CODE BEGIN CLK 1 */
/* The system Clock is configured as follows :
CPU Clock source = IC1_CK
System bus Clock source = IC2_IC6_IC11_CK
CPUCLK (sysa_ck) (Hz) = 600000000
SYSCLK AXI (sysb_ck) (Hz) = 400000000
SYSCLK NPU (sysc_ck) (Hz) = 300000000
SYSCLK AXISRAM3/4/5/6 (sysd_ck) (Hz) = 400000000
HCLKx(Hz) = 200000000
PCLKx(Hz) = 200000000
AHB Prescaler = 2
APB1 Prescaler = 1
APB2 Prescaler = 1
APB4 Prescaler = 1
APB5 Prescaler = 1
PLL1 State = ON
PLL1 clock source = HSI
PLL1 M = 4
PLL1 N = 75
PLL1 P1 = 1
PLL1 P2 = 1
PLL1 FRACN = 0
PLL2 State = BYPASS
PLL2 clock source = HSI
PLL3 State = BYPASS
PLL3 clock source = HSI
PLL4 State = BYPASS
PLL4 clock source = HSI
*/
/* USER CODE END CLK 1 */
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the System Power Supply
*/
if (HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY) != HAL_OK)
{
Error_Handler();
}
/* Enable HSI */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Get current CPU/System buses clocks configuration and if necessary switch
to intermediate HSI clock to ensure target clock can be set
*/
HAL_RCC_GetClockConfig(&RCC_ClkInitStruct);
if ((RCC_ClkInitStruct.CPUCLKSource == RCC_CPUCLKSOURCE_IC1) ||
(RCC_ClkInitStruct.SYSCLKSource == RCC_SYSCLKSOURCE_IC2_IC6_IC11))
{
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_SYSCLK);
RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_NONE;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL1.PLLM = 4;
RCC_OscInitStruct.PLL1.PLLN = 75;
RCC_OscInitStruct.PLL1.PLLFractional = 0;
RCC_OscInitStruct.PLL1.PLLP1 = 1;
RCC_OscInitStruct.PLL1.PLLP2 = 1;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_CPUCLK|RCC_CLOCKTYPE_HCLK
|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
|RCC_CLOCKTYPE_PCLK2|RCC_CLOCKTYPE_PCLK5
|RCC_CLOCKTYPE_PCLK4;
RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_IC1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_IC2_IC6_IC11;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
RCC_ClkInitStruct.APB5CLKDivider = RCC_APB5_DIV1;
RCC_ClkInitStruct.IC1Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC1Selection.ClockDivider = 2;
RCC_ClkInitStruct.IC2Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC2Selection.ClockDivider = 3;
RCC_ClkInitStruct.IC6Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC6Selection.ClockDivider = 4;
RCC_ClkInitStruct.IC11Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC11Selection.ClockDivider = 3;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief NVIC Configuration.
* @retval None
*/
static void MX_NVIC_Init(void)
{
/* EXTI13_IRQn interrupt configuration */
HAL_NVIC_SetPriority(EXTI13_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI13_IRQn);
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOO_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
/*Configure the EXTI line attribute */
HAL_EXTI_ConfigLineAttributes(EXTI_LINE_13, EXTI_LINE_SEC);
/*Configure GPIO pin : BP1_Pin */
GPIO_InitStruct.Pin = BP1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(BP1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : LED1_Pin */
GPIO_InitStruct.Pin = LED1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LED1_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
HAL_GPIO_TogglePin(LED1_GPIO_Port,LED1_Pin);
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Solved! Go to Solution.
2025-10-01 9:14 AM
Hello @emmanuel_, and welcome to ST Community!
In your callback function, you need to add an if statement to check the pin source of the external interrupt, which in your case will be triggered by the User button.
If you get stuck, you can refer to the CubeN6 firmware repository located here:
C:\Users\%USERNAME%\STM32Cube\Repository\STM32Cube_FW_N6_V1.2.0\Projects\NUCLEO-N657X0-Q
Alternatively, you can check the project I attached below. Feel free to ask any questions.
Best regards,
2025-10-01 9:14 AM
Hello @emmanuel_, and welcome to ST Community!
In your callback function, you need to add an if statement to check the pin source of the external interrupt, which in your case will be triggered by the User button.
If you get stuck, you can refer to the CubeN6 firmware repository located here:
C:\Users\%USERNAME%\STM32Cube\Repository\STM32Cube_FW_N6_V1.2.0\Projects\NUCLEO-N657X0-Q
Alternatively, you can check the project I attached below. Feel free to ask any questions.
Best regards,
2025-10-02 9:32 AM
Hello @STackPointer64 ,
I'm very happy , Thank you very much for your help. My code is now working perfectly and I will be able to move forward with my project!
Cheers
Emmanuel
2025-10-02 9:34 AM
You’re most welcome! If you encounter any other issues, please feel free to ask your questions on the community. Have a great day!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.