2019-06-10 7:32 AM
Hello, Community.
I am currently trying to control a power converter with a STM32F4 microcontroller. The thing is that the control variable is the frequency of the PWM. I have programmed a timer (TIM3) that generates an interruption every 100us. During this interruption, the MCU has to calculate the new frequency value of the PWM in order to switch the power MOSFET.
I tried two options but none of them work as I want.
case a) Modifying the ARR register on the fly.
If I do this, I have seen that many times, the PWM doesn't work and remains at high level during a certain time (400us or so). Please, kindly see the yellow pulses. It obviously has effects over the power converter.
case b) I thought that since the register is not updated inmediately, I could reset the counter of the PWM timer. This time, the PWM no longer remains high during a certain time but it provides strange pulses.
TIM8 -> CNT = 0;
TIM8->ARR = "calculated value"; I read about diferent registers to make the updates of the registers inmediately but I am not capable. I tried many things but they don't work.
Could you give me a hint? Thanks a lot.
2019-06-11 12:38 AM
Thanks to all
2022-12-21 11:19 PM
Greetings ,
Can you please explain how did u achive your goal ? I am doing as below
while (1)
{
HAL_Delay(2000);
//TIM5->ARR = _arr;
//TIM5->CCR1 = _arr / 2;
while(__HAL_TIM_GET_COUNTER(&htim5) < _arr);
HAL_TIM_PWM_Stop(&htim5, TIM_CHANNEL_1);
_pwm_freq += 10;
_arr = _pwm_timer_freq / _pwm_freq;
_ccr = _arr / 2;
__HAL_TIM_SET_AUTORELOAD( &htim5, _arr );
__HAL_TIM_SET_COMPARE(&htim5, TIM_CHANNEL_1, _ccr);
HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_1);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.