2026-03-24 1:06 AM
Hello to the STM32 Community,
I am trying to connect a fast TI DAC904 to a Nucleo board with H743. I am using it as a single M7 core. I have built a project with CubeMX where:
Timer1 -> DMA -> FMC -> DAC904
Short sine buffer in RAM-D1 and DMA as circular buffer
It works but I am getting maximum speed of 12.6 MSps.
I have tried to modify the timer frequency but I am getting a limit at that speed
Is there a way to make if faster?
Thank you
Benny
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.