STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Modify PWM frequency on the fly (STM32F4)

Hello, Community.I am currently trying to control a power converter with a STM32F4 microcontroller. The thing is that the control variable is the frequency of the PWM. I have programmed a timer (TIM3) that generates an interruption every 100us. Durin...

0690X000008iQqvQAE.jpg 0690X000008iQrPQAU.jpg

Unable to get 0 or 100% duty cycle in up-counter mode

Dear community I am new STM32G4 family bu i have several years of experience with C2000 form competitor TI. I would like to use STM32G4 controller in new project but i have lots of problems. I have read AN4539 HRTIM cookbook and HRTIM chapter in Refe...

PBana.2 by Associate
  • 1979 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H750 uart problem

Hi, may i know how to use the uart using stm32h750. I just try using the basic uart application which is hello world but nothing show up. I literally follow same setting with nucleo board for uart. but it does not working with stm32h750? May i know i...

Angle by Associate II
  • 4027 Views
  • 7 replies
  • 0 kudos

Is the bootloader host code available in some form?

I am working on a project where several STM32L0xx processors will be running under a Raspberry Pi 4+ system. The desire is to be able to use the SystemBootloader on these to be able to do firmware updates. I know that the documentation from ST is eno...

DavePfz by Associate III
  • 2799 Views
  • 2 replies
  • 0 kudos

Generating a DFU file from Hex from bat

I want to be able to run a bat file that has inside it the path to a hex file. When i run it, it converts it to a dfu file, without the user needing to do any more clicks or inputs. I tried to do this by using encedo's hex2dfu from github. The proble...

KHans.5 by Associate
  • 1997 Views
  • 1 replies
  • 0 kudos

Resolved! Error in STM32F769 Reference manual RM0410 Rev4

Hello there,recently I have found an error in the reference manual RM0410.On page 1546 in figure 503 Filtering mechanism - example it is Identifier #4, which matches the recevied message. However, in the description below it said Identifier #2. I don...

JPan.4 by Associate III
  • 1104 Views
  • 2 replies
  • 1 kudos

Resolved! Noise in the open colector output

Hello guys, I have a problem with my project. I'm development the PS/2 (device, keyboard-like) protocol with my STM32F103C8T6 (Bluepill). When i convert my port to the open collector output, the noise appear in the PS/2 bus. In this moment, the STM32...

0693W00000WLT39QAH.png 0693W00000WLT3EQAX.png 0693W00000WLT3xQAH.png

STM32U585 - Wakeup reason detection when exiting shutdown

Hi, Im trying to get WUP reason after the MCU exited the shutdown. I'm using pushbutton connected to PC5 pin to wake up the MCU. I cannot get the WUP flag to behave correctly. Sometimes it is present, sometimes not. This feature is part of bigger pro...

DHečk.1 by Associate
  • 2154 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.