2023-11-06 5:34 PM
i want to measure the power consumption of my stm32f769 discovery board, while its runs a simple NN model. Is there any way to do it using the STMCubeMX? or do i need to get a X-NUCLEO-LPM01A power shield? If so, would that be compatible with the STM32F769I-DISCO? @Stephanie Low @FBL
2023-11-07 12:51 AM
Hi @aben118,
yes, you need the X-NUCLEO-LPM01A power shield, which is compatible thanks to the Arduino connector. Then, you can monitor power with STM32CubeMonitor-Power (link).
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.