STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CRS SYNC setup with LSE and CubeMX puzzle

I try to setup CRS SYNC setup with LSE using the latest CubeMX.It appears that when CRS SYNC with Source LSE is selected, LSE does not get initialized unless RTC is active as well and its clock source is set to LSE. E.g crystal drive level option doe...

RCC-A.png RCC-B.png RCC-C.png
TDJ by Lead
  • 3333 Views
  • 2 replies
  • 3 kudos

Compatible SDIO voltage translator for STM32F413

Hi,We are designing STM32F413ZHJ6 at 1.8V and are looking for a suitable level translator to 3.3V for the on-board microSD connector. I'm considering NXS0506UP or NVT4858. Just wondering if these parts would be compatible with the STM32? Any suggesti...

Thai by Associate
  • 2605 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H5 Need bootloader pins

As per errors in AN2606 and this thread https://community.st.com/t5/stm32-mcus-products/stm32h5-bootloader-uses-usart-pins-that-do-not-match-roles-in/m-p/594610#M224078 I need the correct pins that STM32H563/STM32H573 use for USART1/2/3 and FD-CAN bo...

MBC by Associate III
  • 6061 Views
  • 6 replies
  • 3 kudos

measure power consumption of STM32F769I-DISCO

i want to measure the power consumption of my stm32f769 discovery board, while its runs a simple NN model. Is there any way to do it using the STMCubeMX? or do i need to get a X-NUCLEO-LPM01A power shield? If so, would that be compatible with the STM...

aben118 by Associate II
  • 2082 Views
  • 1 replies
  • 0 kudos

Mysterious noise on ADC

Hello everyone,I’m currently developing a device that collects surface electromyography (EMG) signals in the abdominal region. The device works as follows:Uses the AD8232 IC to collect the EMG data.Connects the output EMG signal to our MCU's internal...

plots.png
MAndr.233 by Associate III
  • 1919 Views
  • 1 replies
  • 0 kudos

Resolved! Executing code in external OCTO SPI-flash for H7-device?

 Hi!I have a TouchGFX project based on a H725-device with a large display 1024x600 having a fair amount of graphic components. It is a custom board but I am using STM32H735G-DK as a reference.I have two related questions before moving onwards:1. Appl...

STM32F0RB Discovery Board

Hi, I am new to work on STM32F0 discovery board. I am Implementing the USB communication TX/RX with iMX8 controller. I am trying to send  and receive the 65 bytes of data packet, but it is communicating only 64 bytes of data packet, as its implemente...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.