2015-01-27 10:59 AM
Hello,
Based on this very good example (below from clive1) on how to set up the timers for low frequencies, I'm trying to now adjust the PWM signal from each output. Note that the configuration has only the mode changed from ''TIM_OCMode_Toggle'' to ''TIM_OCMode_PWM1'' which now generates the PWM signals. To create the duty cycle, I did this: TIM_OCInitStructure.TIM_Pulse = (uint16_t)(Period * dutyCycle); Where dutyCycle is a value between 0.1 and 0.5, it works fine. However, what I really need is the second channel to have exactly the same duty cycle, but offset by some interval in milliseconds (or ratio of period), this to drive an H-Bridge. The only result I can get is that the second channel just changes the duty cycle. Is there any way to do this in one setup, or do I need another Timer set up the same way and trigger the second one relative to the first? (see comments in sample below) Thank you! Help appreciated as always. /********************************************************************/void TIM4_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
int Prescaler, Period;
Prescaler = ((SystemCoreClock / 2) / 20000); // 20 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
Period = 20000 / 1; // 1 Hz - 1 second on, 1 second off duty
// The toggle halves the frequency, a phase shift of 90 degrees (1/4) is 180 degrees (1/2)
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
/* Output Compare Toggle Mode configuration: Channel 1, 2 & 3 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_Pulse = (uint16_t)(Period * dutyCycle);
TIM_OC1Init(TIM4, &TIM_OCInitStructure);
TIM_OCInitStructure.TIM_Pulse = ????? - NEED SAME DUTY CYCLE BUT LAGGING CHANNEL 1
TIM_OC2Init(TIM4, &TIM_OCInitStructure);
/* TIM4 enable counter */
TIM_Cmd(TIM4, ENABLE);
}
#stm32f4-timers-pmw
2015-01-27 12:41 PM
This wades off in to areas of the timer design I really don't like, or understand well. Or may be I understand they don't work well...
I'd perhaps try using two timers of identical configuration, and achieve the phase shift via different TIMx->CNT settings with the desired offset. Then enable both with some tight code. There are perhaps ways to get a common trigger or sync. But you'd probably not want a reset.2015-01-27 1:33 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.