STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube HAL documentation

Posted on January 28, 2015 at 09:32Hello,Where can we find documentation for STM32F HAL API, generated by Cube?Thanks!

George.P by Associate III
  • 1254 Views
  • 2 replies
  • 0 kudos

USART HalfDuplex (Rx/Tx) and Rx Funktion

Posted on January 27, 2015 at 16:05Hello, is it possible to use one USART in HalfDuplexMode (Rx and Tx via Tx Pin) AND the Rx Pin of the same USART to receive another stream? regards Florian

f2 by Associate II
  • 1496 Views
  • 2 replies
  • 0 kudos

UART problem with STM32 discovery kit (MB913C)

Posted on January 28, 2015 at 05:53Hello, I'm in the midst of project development using STM32F100RBx discovery kit (MB913C) and generating code by using STM32CubeMX and configure USART1 as asynchronous. I use Keil Arm-MDK and trying use ''HAL_UART_T...

lcd segment & i2c stm32l053

Posted on January 28, 2015 at 02:07I created a project by STM32cubeMX, the project has : I2C communication with sensor, display data by LCD segment:int main(void){  MX_GPIO_Init();  MX_I2C1_Init();    MX_LCD_Init();..........But, when have  MX_LCD_I...

Storage Temperature of STM32F103RGT7

Posted on January 13, 2015 at 22:01Hello, I am currently using STM32F103RGT7 to control my BLDC motors. I am suppose to sterilize the PCB which has the controller mounted on it in an Autoclave (steam sterilization). During which the controller will ...

DfuSe doesn't work

Posted on January 26, 2015 at 01:42 I down load a DfuSe demo, but it can not read a *.hex file.

Linda by Associate II
  • 2052 Views
  • 5 replies
  • 0 kudos

STM32F429DISO connection failed

Posted on January 26, 2015 at 21:27Hello, I hope you can help me. A long time I flashed and debugged my STM32F429DISC. And then the connection failed, the IDE (coocox) said, I should to check the cable connection. I tried to use an other program CoF...

0690X00000605WRQAY.png 0690X00000605ZyQAI.png 0690X00000603KwQAI.jpg 0690X00000605ZFQAY.png
der-kyle by Associate II
  • 2112 Views
  • 4 replies
  • 0 kudos

STM32F429 Discovery Board SDRAM

Posted on January 27, 2015 at 20:07 Good evening, i am a beginner in the stm32f microcontroller and i am trying to learn how to use the SDRAM embedded on the discovery board.I made a function which initialize the sdram gpio and timing characteri...

Stm32f407 httpserver project allowed code size problem

Posted on January 27, 2015 at 16:01Hi, I want to use webserver connection with stm32f407 and i found this and downloaded :http://www.st.com/web/en/catalog/tools/PF257906 I'm using keil uvision 5 and trying to build the httpserver project but i'm get...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.