2020-06-24 4:41 AM - last edited on 2023-09-01 9:47 AM by Amel NASRI
I am using STM32F407 Discovery Board and I'm generating my project using MX Cube
I'm doing testing on I2C sensor that is MLX 640 which is used for taking thermal image , so basically we are are reading frames of thermal image via I2C on every 1 second and doing some processing on it. Basically some floating operations on each frames
The data sheet of MLX 640 -https://www.melexis.com/-/media/files/documents/datasheets/mlx90614-datasheet-melexis.pdf
So while doing this initially all floating operations are done by STM for few frames , but after few frames we are getting HAL I2C error that is 0x02 i.e HAL_BUSY
HAL_OK = 0x00U,
HAL_ERROR = 0x01U,
HAL_BUSY = 0x02U,
HAL_TIMEOUT = 0x03U
and it's getting stuck every single time
What type of thing should I do for I2C to not get busy and it works properly for each frame with all floating operations.
Should I try to reset I2C after each frame? If yes, then how am I suppose to do that?
And If no, then what is the way to do it?
2020-06-24 8:39 PM
HAL_BUSY means either the peripheral isn't ready because you're using it somewhere else, or the line is busy. If it's the former, fix your code. If it's the latter, a device may be holding down the SCL line, or the STM32 I2C peripheral is just in a bad state. You can try to reset the peripheral to see if it frees up. You can reset the peripheral with the I2C_CR1_SWRST bit.
In either case, it shouldn't be happening and you should figure out the cause. I would attach a logic analyzer and see if I could spot the issue and go from there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.