STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C BUSY

I am using STM32F407 Discovery Board and I'm generating my project using MX Cube   I'm doing testing on I2C sensor that is MLX 640 which is used for taking thermal image , so basically we are are reading frames of thermal image via I2C on every 1 sec...

Djain.1 by Associate II
  • 7680 Views
  • 1 replies
  • 1 kudos

LSE clock start-up problem

Hi, i'm trying to use the LSE clock with the RTC but it doesn't start until i make a state reset or run the code under debug mode.I have read all other posts of LSE problems in the forum and found a lot of info, almost everything related with hardwar...

0693W000001rOw9QAE.png 0693W000001rOwdQAE.png 0693W000001rOwsQAE.png 0693W000001rOx2QAE.png
TOrdó.1 by Associate
  • 4037 Views
  • 4 replies
  • 0 kudos

Use timer`s chain to generate N impulse`s

I do some serial interface clock with timers chain on stm32f407.Thats work, but generate little bit lower count of impulses. where is my trouble? len is about 16 384, overall pulse count len*16.I miss about 200*16=3200 pulses.Thank You!TIM2->PSC=0;  ...

AlexKeisy by Associate III
  • 3387 Views
  • 7 replies
  • 1 kudos

Real time debugger needed

Hi, Currently i am using STM32L082CZ processor and debugger tools as ST-LINK V2 B2019-51.When I enter debug mode, it will update the status/flag/watch variable upon reach breakpoints. The debugger window show on Keil won't update during run time, i...

JChew.1 by Associate II
  • 1934 Views
  • 3 replies
  • 0 kudos

Strange behavior of PWM

Hello,​I​ am observing a strange behaviour of the first few PWM pulses after a change in duty cycle. I use HAL_TIM_PWM_Stop, HAL_TIM_ConfigChannel (with the changed Pulse) and then HAL_TIM_PWM_Start. What happens is that for around 1 millisecond the ...

JWilk.1 by Associate II
  • 11347 Views
  • 10 replies
  • 0 kudos

External interrupts

The line where the external interrupt is set  SYSCFG->EXTICR [2] |= (3 << 12); I want to set it for port D pin 10. How the masking and unmasking is done for port D?

Nmv1608 by Associate II
  • 2354 Views
  • 4 replies
  • 0 kudos

STM32F103RCT6 HSE and LSE Crystal selection

Hi,I am designing a st board for the first time. First, we made all the improvements on the blue pill, which is STM32F103C8T6. When this wasn't enough, we switched to STM32F103RCT6.I am currently drawing a schematic of this card and was confused in ...

0693W000001plN3QAI.jpg 0693W000001plNNQAY.jpg 0693W000001plNmQAI.jpg
Meyup by Associate II
  • 3701 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.