2017-11-12 7:07 PM
hi 12864L LCD sample source is being applied.
I want to change to hal lib because the old source has already been created.Help!
//-------------------------------------------------------------------------------------------------
// Universal KS0108 driver library// STM32 MCU low-level driver// (c) Rados³aw Kwiecieñ,
mailto:radek@dxp.pl
//-------------------------------------------------------------------------------------------------#include 'main.h'
#define KS0108_PORT GPIOE
#define KS0108_RS GPIO_Pin_8
#define KS0108_RW GPIO_Pin_9#define KS0108_EN GPIO_Pin_10#define KS0108_CS1 GPIO_Pin_11
#define KS0108_CS2 GPIO_Pin_12#define KS0108_CS3 GPIO_Pin_13#define KS0108_D0 0
#define DISPLAY_STATUS_BUSY 0x80
extern unsigned char screen_x;
extern unsigned char screen_y;LL_GPIO_InitTypeDef GPIO_InitStructure;
//-------------------------------------------------------------------------------------------------
// Delay function /for 8MHz///-------------------------------------------------------------------------------------------------void GLCD_Delay(void){ asm('nop');asm('nop');asm('nop');asm('nop');}//-------------------------------------------------------------------------------------------------// Enalbe Controller (0-2)//-------------------------------------------------------------------------------------------------void GLCD_EnableController(unsigned char controller){switch(controller){ case 0 : GPIO_ResetBits(KS0108_PORT, KS0108_CS1); break; case 1 : GPIO_ResetBits(KS0108_PORT, KS0108_CS2); break; case 2 : GPIO_ResetBits(KS0108_PORT, KS0108_CS3); break; }}//-------------------------------------------------------------------------------------------------// Disable Controller (0-2)//-------------------------------------------------------------------------------------------------void GLCD_DisableController(unsigned char controller){switch(controller){ case 0 : GPIO_SetBits(KS0108_PORT, KS0108_CS1); break; case 1 : GPIO_SetBits(KS0108_PORT, KS0108_CS2); break; case 2 : GPIO_SetBits(KS0108_PORT, KS0108_CS3); break; }}//-------------------------------------------------------------------------------------------------// Read Status byte from specified controller (0-2)//-------------------------------------------------------------------------------------------------unsigned char GLCD_ReadStatus(unsigned char controller){unsigned char status;GPIO_StructInit(&GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = 0xFF << KS0108_D0;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;GPIO_Init(KS0108_PORT, &GPIO_InitStructure);GPIO_SetBits(KS0108_PORT, KS0108_RW);
GPIO_ResetBits(KS0108_PORT, KS0108_RS);GLCD_EnableController(controller);GLCD_Delay();GPIO_SetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();status = ((GPIO_ReadInputData(KS0108_PORT) >> KS0108_D0) & 0xFF);GPIO_ResetBits(KS0108_PORT, KS0108_EN);GLCD_DisableController(controller);return status;}//-------------------------------------------------------------------------------------------------// Write command to specified controller//-------------------------------------------------------------------------------------------------void GLCD_WriteCommand(unsigned char commandToWrite, unsigned char controller){while(GLCD_ReadStatus(controller)&DISPLAY_STATUS_BUSY);GPIO_StructInit(&GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = (0xFF << KS0108_D0);GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;GPIO_Init(KS0108_PORT, &GPIO_InitStructure);GPIO_ResetBits(KS0108_PORT, KS0108_RS | KS0108_RW);
GLCD_Delay();GLCD_EnableController(controller);GLCD_Delay();GPIO_SetBits(KS0108_PORT, (commandToWrite << KS0108_D0));commandToWrite ^= 0xFF;GPIO_ResetBits(KS0108_PORT, (commandToWrite << KS0108_D0));GLCD_Delay();GPIO_SetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();GPIO_ResetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();GLCD_DisableController(controller);}//-------------------------------------------------------------------------------------------------
// Read data from current position//-------------------------------------------------------------------------------------------------unsigned char GLCD_ReadData(void){unsigned char tmp;while(GLCD_ReadStatus(screen_x / 64)&DISPLAY_STATUS_BUSY);GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = 0xFF << KS0108_D0;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;GPIO_Init(KS0108_PORT, &GPIO_InitStructure);GPIO_SetBits(KS0108_PORT, KS0108_RS | KS0108_RW);
GLCD_EnableController(screen_x / 64);
GLCD_Delay();GPIO_SetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();tmp = ((GPIO_ReadInputData(KS0108_PORT) >> KS0108_D0) & 0xFF);GPIO_ResetBits(KS0108_PORT, KS0108_EN);GLCD_DisableController(screen_x / 64);screen_x++;return tmp;}//-------------------------------------------------------------------------------------------------// Write data to current position//-------------------------------------------------------------------------------------------------void GLCD_WriteData(unsigned char dataToWrite){while(GLCD_ReadStatus(screen_x / 64)&DISPLAY_STATUS_BUSY); GPIO_StructInit(&GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = (0xFF << KS0108_D0);GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;GPIO_Init(KS0108_PORT, &GPIO_InitStructure);GPIO_ResetBits(KS0108_PORT, KS0108_RW);
GLCD_Delay();GPIO_SetBits(KS0108_PORT, KS0108_RS);GLCD_Delay();GPIO_SetBits(KS0108_PORT, (dataToWrite << KS0108_D0));dataToWrite ^= 0xFF;GPIO_ResetBits(KS0108_PORT, (dataToWrite << KS0108_D0));GLCD_Delay();GLCD_EnableController(screen_x / 64);GLCD_Delay();GPIO_SetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();GPIO_ResetBits(KS0108_PORT, KS0108_EN);GLCD_Delay();GLCD_DisableController(screen_x / 64);screen_x++;}//-------------------------------------------------------------------------------------------------////-------------------------------------------------------------------------------------------------void GLCD_InitializePorts(void){vu32 i;RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE);
GPIO_StructInit(&GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;GPIO_Init(KS0108_PORT, &GPIO_InitStructure);
GPIO_Write(KS0108_PORT, KS0108_CS1 | KS0108_CS2 | KS0108_CS3 | KS0108_RS | KS0108_RW | (0xFF << KS0108_D0));}//-------------------------------------------------------------------------------------------------////-------------------------------------------------------------------------------------------------unsigned char GLCD_ReadByteFromROMMemory(char * ptr){ return *(ptr);}//-------------------------------------------------------------------------------------------------////-------------------------------------------------------------------------------------------------2017-11-13 1:15 PM
It's just GPIO manipulation. It should be easy to replace the SPL functions with their Cube/HAL counterparts.
The original author may be available to provide some support in case of problems, try to contact him.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.