STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB VCP problem under Windows 10

Posted on November 14, 2017 at 01:25Hi,i use STM32F107RB in my project wherein is an USB VCP virtual com port driver (The basic of the USB VCP is the STM3210C-EVAL_USB_decice_VCP example of the Atollic True Studio). It works well if i use under Wind...

STM32L486 VREFBUF precision

Posted on November 13, 2017 at 09:42We have build some prototypes of  a new product containing the STM32L486 (UFBGA132 package). The VREF+ pin is buffered with 1µF and 100nF. I measured the reference voltage with two different calibrated multimeter...

When to set TIM1 pwm channels - 3phase drive

Posted on November 13, 2017 at 20:52Hello,I have a  project where a 3phase DC BLDC motor is required to be spined.For now i have : - 3 hall sensors conected to CH1,2,3 of the TIMER2.                          - 6 complementary pwms via Timer1In the T...

Bogdan by Senior
  • 747 Views
  • 0 replies
  • 0 kudos

problem with IAR debug(?)

Posted on November 13, 2017 at 17:09hi. when i am debuging my code in IAR , debug 's Arrow  go to Disassembly and i cant continue debug, beacuse i think the arrow stop at that line.and i want debugger do line by line in my code and never go to the D...

_legacyfs_online_stmicro_images_0690X0000060MxqQAE.png

Duty cycle of PWM unstable

Posted on November 13, 2017 at 13:29I have a problem with PWM generation.I have my own PCB with the uC STM32F429IIH. I am trying to configure the PWM in TIM3 channel 1. My clock frecuency is 180 MHz and APB1 Timer Clock is 90 MHz.I use STM32CubeMX t...

''Safe'' version of HAL_GetTick()?

Posted on November 09, 2017 at 21:04Using the STM32F413 Nucleo-144 and STM32F091 Nucleo-64 evaluation boards. I am using a combination of HAL_GetTick() and a read of the countdown timer to generate higher resolution time stamps for events. Using the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.