2018-03-08 9:08 AM
Good evening,
I've been developing a solution using two SP1MLs to control a quadcopter. I'm using MAVLink as the protocol, however I've been getting too high packet losses between the ground station and quadcopter. Both sides use DMA with double-buffering to read the UART, so the problem probably lies in the wireless link. The problem is that both sides must stream data continuously, according to the following scheme:
Quadcopter ? Ground station
MessageSizeInterval
Heartbeat17 bytes1000 ms
Attitude40 bytes50 ms
Obstacles22 bytes50 ms
Ground station ?Quadcopter
MessageSizeInterval
Heartbeat17 bytes1000 ms
Manual control19 bytes20 ms
Misc params?? bytesOn user request
This scheme works fine when only one side is transmitting, however when both are enabled I have over 90% packet loss. The quadcopter is already waiting for the IDLE flag to transmit, however the problem still persists. The relevant configurations are:
ParamValue
Frequency915MHz
Modulation2-FSK
Data rate150kbps
Baud rate
115200
Frequency deviation
300kHz
Filter
500kHz
FEC
Enabled
Based on that, my questions are:
Thanks in advance,
Pedro
(Sorry for any mistake, English is not my native language)
#sp1ml-spirit1-stm32l1-sub-ghz #stm-32 #stm32-projects #sp1ml2018-03-08 12:51 PM
What is an '
SP1ML' ?
EDIT
Oh - you mean this:
http://www.st.com/en/wireless-connectivity/sp1ml.html
?Why would Google not find that just now?
2018-03-08 2:06 PM
The radio always prevails as the biggest source of data loss. On some other boards the HAL and CM0 architecture can also manage to corrupt things.
From a radio perspective I've found the Semtech LoRa radio chips (SX1272, 1276 primarily) to be significantly more robust than other sub-1GHz solutions (Si1000, EZR, etc). The Murata LoRa module integrates a very capable STM32L072CZ with 192KB of FLASH, which can hold the entire radio stack and user application. It uses a TCXO, so good on-frequency design, with good sensitivity.
There are dozens of SX127x based radio modules, and Semtech is working with number of licensees.
2018-03-08 2:48 PM
Yup, these are the modules I'm talking about. They are NRND now, but weren't when I started using them.
2018-03-08 10:54 PM
This scheme works fine when only one side is transmitting, however when both are enabled I have over 90% packet loss.
First, I would try to find out why you are losing packets.
Are the data corrupted, or can't your code keep up (i.e. is the OVL flag set, or an error flag) ?
Second, DMA seems not appropriate for variable-length packets.
And what happens to your application timing logic if one character is lost or corrupted ?
2018-03-08 11:43 PM
This scheme works fine when only one side is transmitting,
however when both are enabled I have over 90% packet loss.
Are these devices actually designed for full-duplex operation?
Usually, that would require a different frequency for 'uplink' and 'downlink' - otherwise they will interfere with each other ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.