STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot install STM32 Cube programmer for MAC

Posted on February 12, 2018 at 15:54Hello, I'm having troubles installing STM32Cube Programmer under MAC - High Sierra, recently formatted.The installation process starts regularly and then freezes forever!Can anyone help me??Regards :)

STM32L432 LSE startup timeout with CSS enabled

Posted on March 09, 2018 at 08:35if Clock security system on LSE is enabled:After a few power on/off/on cycles, Clock security system protection always is triggered.  Only power off for more 5s will reset protection bit.Currently I disabled clock se...

Darius B by Associate II
  • 903 Views
  • 0 replies
  • 0 kudos

How to implement the X-NUCLEO-IDB05A1 properly

Posted on March 09, 2018 at 00:22I am working on a project which demands a BTLE connection due to energy constraints and i am having trouble using the btle shield mentioned in the title.Is there a proper way to implement the drivers and using cubemx...

STM Studio: gdb parse error ?

Posted on November 14, 2017 at 22:33 Hi ! Using STM Studio with my current project gives me 2 errors while loading the elf file: Seems to be parsing problem of the used gdb.exe tool. As a result the provided symbol list is very small .....

0690X0000060PEKQA2.png 0690X0000060PELQA2.png 0690X0000060PD4QAM.png

Disabling FreeRTOS and entering standby mode

Posted on March 07, 2018 at 22:43I am using STM32L053 and Keil IDE. I have imported FreeRTOS from CubeMX. Is there a way I could disable the FreeRTOS and enter into standby mode? Then, wake up on GPIO signal (external interrupt). And when I wake up,...

Jagadish by Associate II
  • 3848 Views
  • 5 replies
  • 0 kudos

STM32L4 keep pin high in StandBy mode?

Posted on November 03, 2017 at 17:53Hi,I work on design with STM32L452RET6P and I'm considering power managment. I've got some voltage regulators that needs high voltage on SHDN pin and i want to use GPIO to keep this regulators on. I have read data...

misiael by Associate
  • 3853 Views
  • 3 replies
  • 0 kudos

Static and Dynamic analysis tools

Posted on March 08, 2018 at 16:38Hi STM community,  I want to run valgrind and lint as part of static and dynamic code analysis.I tried to run valgrind option in system work bench IDE , But it is giving the following errorvalgrind: failed to start t...

Keil v6 compiler and STM32F3xx MXCUbe code, FPUs

Posted on March 08, 2018 at 13:33Folks again problem with the Keil V6 compiler and ST source codeSo code from mxCube v4.24.0the F3 lib is 1.9using Keil 5.25 with the project settings modified to the V6.9 compiler and the FPU of the F3 micro is enabl...

dcurran2 by Associate II
  • 1688 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.