2014-05-04 7:04 AM
Hello,
I am trying to get double buffered USB bulk-out transfers working.The device does enumerate correctly but bulk transfers do not even raise interrupts. This is my EP initialization (usb_prop.c : reset handler: [code] SetBTABLE(BTABLE_ADDRESS); // ======================================================== // Initialize Endpoint 0 // ======================================================== SetEPType(ENDP0, EP_CONTROL); SetEPTxStatus(ENDP0, EP_TX_NAK);//STALL); SetEPRxAddr(ENDP0, ENDP0_RXADDR); SetEPRxCount(ENDP0, Device_Property.MaxPacketSize); SetEPTxAddr(ENDP0, ENDP0_TXADDR); Clear_Status_Out(ENDP0); SetEPRxValid(ENDP0); // ======================================================== // Initialize Endpoint 1 - tx - IN // ======================================================== SetEPType(ENDP1, EP_BULK); SetEPDoubleBuff(ENDP1); SetEPDblBuffAddr (ENDP1, ENDP1_BUF0_ADDR, ENDP1_BUF1_ADDR); SetEPDblBuffCount(ENDP1, EP_DBUF_IN, 0x40); ClearDTOG_RX(ENDP1); ClearDTOG_TX(ENDP1); ToggleDTOG_TX(ENDP1); SetEPTxStatus(ENDP1, EP_TX_NAK); SetEPRxStatus(ENDP1, EP_RX_DIS); // ======================================================== // Initialize Endpoint 2 - rx - OUT // ======================================================== SetEPType(ENDP2, EP_BULK); SetEPDoubleBuff(ENDP2); SetEPDblBuffAddr (ENDP2, ENDP2_BUF0_ADDR, ENDP2_BUF1_ADDR); SetEPDblBuffCount(ENDP2, EP_DBUF_OUT, 0x40); ClearDTOG_RX(ENDP2); ClearDTOG_TX(ENDP2); ToggleDTOG_RX(ENDP2); SetEPRxStatus(ENDP2, EP_RX_VALID); SetEPTxStatus(ENDP2, EP_TX_DIS); SetEPRxValid(ENDP0); SetDeviceAddress(0); bDeviceState = ATTACHED; [/code] register values: USB_EP0R = 00005250 USB_EP1R = 00000161 USB_EP2R = 00007102 CNTR = 0000BF00 ISTR = 00000000 USB_DADDR= 000000A4 BTAB_ADDR= 00000000 PMA BTABLE: 00000080 ADDR0_TX 00000000 COUNT0_TX 00000040 ADDR0_RX 00008400 COUNT0_RX 00000100 ... 00000040 00000140 00000040 00000180 00008400 000001C0 00008400 Device : STM32F103C8T62014-05-04 8:33 AM
ClearDTOG_RX(ENDP2);
ClearDTOG_TX(ENDP2);
ToggleDTOG_RX(ENDP2);
Have you tried not to set the DTOG_RX ?Maybe it will work when started with DTOG cleared.2014-05-04 9:49 AM
Assuming you are working on STM32_USB-FS-Device_Lib_V4.0.0,
// ========================================================
// Initialize Endpoint 2 - rx - OUT
// ========================================================
SetEPType(ENDP2, EP_BULK);
SetEPDoubleBuff(ENDP2);
SetEPDblBuffAddr (ENDP2, ENDP2_BUF0_ADDR, ENDP2_BUF1_ADDR);
SetEPDblBuffCount(ENDP2, EP_DBUF_OUT, 0x40);
ClearDTOG_RX(ENDP2);
ClearDTOG_TX(ENDP2);
ToggleDTOG_RX(ENDP2); // <---- ToggleDTOG_TX(ENDP2);
SetEPRxStatus(ENDP2, EP_RX_VALID);
SetEPTxStatus(ENDP2, EP_TX_DIS);
Tsuneo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.