2026-03-19 4:30 AM - edited 2026-03-19 11:49 AM
Hi ST team,
I am seeing what appears to be a silicon-level issue on STM32H563RGV6, revision X, related to the SWAP_BANK option byte.
When SWAP_BANK is enabled, a USB OUT endpoint stops being re-armed during a flash mass erase of the inactive bank. The USB ISR still executes, but the BULK OUT path wedges because the OUT endpoint is no longer re-armed. Once the mass erase completes, the endpoint behavior returns to normal.
Key observations:
MCU: STM32H563RGV6
Revision: X
The issue is specifically tied to SWAP_BANK being set
The problem occurs during mass erase of the inactive bank
The symptom is specifically USB OUT not being re-armed
This does not look like a total USB interrupt loss; ISR activity can still occur
Other endpoint activity is not affected in the same way
The entire application, including vector table and read-only data used by the relevant path, is relocated to SRAM
Bank selection / inactive-bank arithmetic has been verified and is correct
This does not appear to be a normal software issue. The behavior tracks the SWAP_BANK address remap condition.
My current suspicion is that because SWAP_BANK changes flash address mapping, it may have downstream effects somewhere in the internal address decode / bus matrix / flash-peripheral interaction path during mass erase, and that this is causing the USB OUT endpoint state/update path to fail to reach the condition required for re-arm.
The issue I would like ST to investigate is:
On STM32H563RGV6 revision X, when SWAP_BANK is enabled, a mass erase of the inactive flash bank can cause a USB OUT endpoint to stop being re-armed, even though the system is running entirely from SRAM and inactive-bank selection is correct.
I recognize this is a rare corner case, since many designs would normally pause USB traffic during a flash mass erase. Still, the behavior appears deterministic on STM32H563RGV6 revision X when SWAP_BANK is enabled, so I wanted to report this in case it points to an uncharacterized hardware interaction involving the bank remap.
If useful, I can provide a minimal repro focused specifically on:
STM32H563RGV6 rev X
SWAP_BANK enabled
code / vector table / relevant read-only data all in SRAM
mass erase on inactive bank
active USB OUT traffic during erase
OUT endpoint stops being re-armed until erase completion
Has ST seen this before, or can this be reproduced internally?
Thank you.
2026-04-01 7:11 AM
Hello @KaiY
Thank you for the very detailed analysis and for clearly isolating the conditions of the problem.
To move forward efficiently, the next best step is to reproduce the behavior exactly as you observe it. Could you please share a minimal firmware project to investigate further?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.