STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Who's got success with DCMI ?

Posted on April 28, 2014 at 15:36 Hi there, I am struggling capturing WXGA(1280x1024) images with STMF429 and ov2640 (from STM324x9I-EVAL1 board). SDRAM bandwidth looks just enough to cope with DCMI data and I often catch DMA FIFO errors (sh...

interrupt handling

Posted on March 16, 2012 at 13:33 i am using eCos for my app. i have STM3210E-EVAL board. in my app there is one thread(toggle LED) and external interrupt on PG8. when button is pressed(PG8) another LED should blink once.but nothing... ...

How to program user button interrupt with ecos

Posted on May 03, 2014 at 07:35hi, i'm using a stm32f4 board. and i want to write a program with ecos embeded system that  when i push user button, an interrupt will trigerd and do something. i find the function cyg_interrupt_create(), but i need a ...

huangyg11 by Associate II
  • 2112 Views
  • 4 replies
  • 0 kudos

DAC Software trigger

Posted on May 03, 2014 at 18:56 Hello, somehow i can't find way to do software trigger to start DMA transfer of memory array to dac. Original idea is to fill data array with my wavefrom, and use software trigger to start DMA transfer. Origin...

Temperature sensor in stm32f4-discovery problems

Posted on May 04, 2014 at 09:41Hi everyone, I'm trying to read temperature from temperature sensor in stm32f4-discovery kit I've configured ADC1 and then read converted value and do some math on it now when debugging it goes to hard fault  why ?? I ...

F103 USB BULK OUT Problem

Posted on May 04, 2014 at 16:04Hello, I am trying to get double buffered USB bulk-out transfers working.The device does enumerate correctly but bulk transfers do not even raise interrupts. This is my EP initialization (usb_prop.c : reset handler: [c...

schlenkj by Associate
  • 1340 Views
  • 2 replies
  • 0 kudos

question about DMA

Posted on May 04, 2014 at 16:44I have an ISR, in which a DMA transfer will take place when the ISR is running. Although DMA transfer does not occupy CPU's running time, but occupies the Data bus. So will the DMA's existence lengthen the ISR's execut...

GPIO configuration for LSE crystal (STM32F102RBT6)

Posted on November 28, 2011 at 20:11This should be an easy one for you... I'm a new STM32 user and I am unsure how to configure the GPIO for PC14-15 when using 32kHz crystal as the LSE.  Do both pins need to be configured as alternate function (PP ...

jmorton by Associate II
  • 4090 Views
  • 7 replies
  • 0 kudos

F429 I2C interface init

Posted on May 01, 2014 at 17:52 #include ''stm32f4xx_i2c.h'' #include ''stm32f4xx_rcc.h'' #include ''stm32f4xx_gpio.h'' void I2C1_Init(){ /* Enable Peripheral Clock for I2C1 */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); /* Enable Periph...

kostas by Associate II
  • 3728 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.